<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KWIKSTIK Code for Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497911#M31028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the links, but I have already downloaded projects from the forum, and none of them work to an extend to program a K10 via EZPort.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 13:43:06 GMT</pubDate>
    <dc:creator>donikuy</dc:creator>
    <dc:date>2016-01-20T13:43:06Z</dc:date>
    <item>
      <title>KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497909#M31026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a KWIKSTIK and need to try and use it to download flash image onto a Kinetis MK10 via the EZPort. &lt;/P&gt;&lt;P&gt;Is there any source code available for the KWIKSTIK in order to perform this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 10:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497909#M31026</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2016-01-18T10:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497910#M31027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1" title="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1"&gt;http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4406.pdf?fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1&lt;/A&gt; &lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/598772"&gt;EzPort Cloning&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 14:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497910#M31027</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-18T14:55:55Z</dc:date>
    </item>
    <item>
      <title>Re: KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497911#M31028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the links, but I have already downloaded projects from the forum, and none of them work to an extend to program a K10 via EZPort.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 13:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497911#M31028</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2016-01-20T13:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497912#M31029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can't get project working you can always buy a Dediprog SF600 (for example) since it will usually be cheaper for you if you are a professional developer, rather than investing time building things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 19:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497912#M31029</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-20T19:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497913#M31030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again. I have tried and still no success with the EZPort. Also tried it in another board and it doesn't work. Don't know why it doesn't work, but I suspect it is because when the code was first written it was for coldfire.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason I need this is that our ATE tests and flash downloads the software on the boards in one complete test. This is very efficient, thefore i need the ezprog code to work. Do you thing the Dediprog would be able to do the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber Doniku &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 12:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497913#M31030</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2016-01-22T12:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: KWIKSTIK Code for Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497914#M31031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yiber&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to consult the Dediprogs manual to see whether it would be suitable for your requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The uTasker project includes an EzPort interface that is suitable for all Kinetis parts: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.utasker.com/docs/uTasker/uTaskerEzPortCloner.pdf" rel="nofollow"&gt;http://www.utasker.com/docs/uTasker/uTaskerEzPortCloner.pdf&lt;/A&gt;&lt;SPAN&gt;, allowing both low level and high level programming control, and especially designed for custom Kinetis applications that require testing or programming ability.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The only significant difference between Coldfire and Kinetis EzPort is that the Coldfire needs its Flash clock to be configured and the Kinetis doesn't. This means that Kinetis EzPort is a sub-set of Coldfire EzPort and thus any Coldfire solution should be suitable for Kinetis too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 15:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KWIKSTIK-Code-for-Kinetis/m-p/497914#M31031</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-22T15:29:45Z</dc:date>
    </item>
  </channel>
</rss>