<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックmk22fn512 dac output</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494803#M30715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to K series processors and i selected "mk22fn512vlh12" 64 LQFP for a new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to have two independent DAC outputs besides at least two ADC inputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been reading several docs that says that this part has 2x DAC (12bit) however i can't find the pin of the second DAC output on the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the datasheet: "k22p121m120sf7.pdf" on page 63 table i see that DAC0 is on pin 18, but DAC1 is only on pin k4 of the (121BGA)&amp;nbsp; package, page 73, is this correct ? There isn't DAC1 output for 64LQFP package ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to use a LQFP package, to have 2x DAC and 2x ADC, 2Uarts and SPI, RTC and 128k of flash is enough, i have FRDM-K22F for development, what would be the best part for my project ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your time and attention&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Hugo Nunes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Mar 2016 19:38:37 GMT</pubDate>
    <dc:creator>hancav</dc:creator>
    <dc:date>2016-03-21T19:38:37Z</dc:date>
    <item>
      <title>mk22fn512 dac output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494803#M30715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to K series processors and i selected "mk22fn512vlh12" 64 LQFP for a new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to have two independent DAC outputs besides at least two ADC inputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been reading several docs that says that this part has 2x DAC (12bit) however i can't find the pin of the second DAC output on the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the datasheet: "k22p121m120sf7.pdf" on page 63 table i see that DAC0 is on pin 18, but DAC1 is only on pin k4 of the (121BGA)&amp;nbsp; package, page 73, is this correct ? There isn't DAC1 output for 64LQFP package ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to use a LQFP package, to have 2x DAC and 2x ADC, 2Uarts and SPI, RTC and 128k of flash is enough, i have FRDM-K22F for development, what would be the best part for my project ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your time and attention&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Hugo Nunes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Mar 2016 19:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494803#M30715</guid>
      <dc:creator>hancav</dc:creator>
      <dc:date>2016-03-21T19:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: mk22fn512 dac output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494804#M30716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hugo,&lt;/P&gt;&lt;P&gt;After have reviewed quite a few reference manual, I think the MK22FN512VLH12 only have the one DAC module.&lt;/P&gt;&lt;P&gt;However I'll confirm it with the AE team later and inform you ASAP if I get the reply.&lt;/P&gt;&lt;P&gt;About your requirement, I'd like to suggest that you can choose the MK24FN1M0VLL12 instead of the MK22FN512VLH12.&lt;/P&gt;&lt;P&gt;And you can learn the more information about the through the link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K24P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K24P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K24P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VE…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 06:14:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494804#M30716</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-03-22T06:14:51Z</dc:date>
    </item>
    <item>
      <title>Re: mk22fn512 dac output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494805#M30717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It would be a great help if you could help me with this doubt.&lt;/P&gt;&lt;P&gt;I would prefer to use mk22fn512 às i have already several resources for it.&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No dia 22/03/2016, às 06:15, jeremyzhou &amp;lt;admin@community.freescale.com&amp;gt; escreveu:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE level="1"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mk22fn512 dac output&lt;/P&gt;&lt;P&gt;reply from jeremyzhou in Kinetis Microcontrollers - View the full discussion&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Hugo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After have reviewed quite a few reference manual, I think the MK22FN512VLH12 only have the one DAC module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I'll confirm it with the AE team later and inform you ASAP if I get the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About your requirement, I'd like to suggest that you can choose the MK24FN1M0VLL12 instead of the MK22FN512VLH12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can learn the more information about the through the link as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K24P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VE…" target="test_blank"&gt;http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K24P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VE…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 11:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mk22fn512-dac-output/m-p/494805#M30717</guid>
      <dc:creator>hancav</dc:creator>
      <dc:date>2016-03-22T11:51:55Z</dc:date>
    </item>
  </channel>
</rss>