<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMKW01xxRM reference manual is missing the I2C chapter</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xxRM-reference-manual-is-missing-the-I2C-chapter/m-p/494700#M30697</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got Rev. 2 - 3/2014 which as far as I can tell is the latest edition. There are numerous references to I2C in the manual (for example section 1.9.2), but no chapter describing the operation or memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is documented elsewhere or if there is a similar I2C peripheral module that I can substitute the documentation for I'd appreciate being directed to that in addition to this manual being updated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Dec 2015 22:12:31 GMT</pubDate>
    <dc:creator>theohill</dc:creator>
    <dc:date>2015-12-17T22:12:31Z</dc:date>
    <item>
      <title>MKW01xxRM reference manual is missing the I2C chapter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xxRM-reference-manual-is-missing-the-I2C-chapter/m-p/494700#M30697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got Rev. 2 - 3/2014 which as far as I can tell is the latest edition. There are numerous references to I2C in the manual (for example section 1.9.2), but no chapter describing the operation or memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is documented elsewhere or if there is a similar I2C peripheral module that I can substitute the documentation for I'd appreciate being directed to that in addition to this manual being updated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 22:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xxRM-reference-manual-is-missing-the-I2C-chapter/m-p/494700#M30697</guid>
      <dc:creator>theohill</dc:creator>
      <dc:date>2015-12-17T22:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: MKW01xxRM reference manual is missing the I2C chapter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xxRM-reference-manual-is-missing-the-I2C-chapter/m-p/494701#M30698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Theo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right, there is a mistake in the MKW01xxRM. I confirm that there are two I2C modules inside the MKW01 MCU, these modules are the same as the included in the KL devices so the information in the &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/KL26P121M48SF4RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/KL26P121M48SF4RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;MKL26 Reference Manual &lt;/A&gt;is valid for this peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl Ramírez.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 23:32:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW01xxRM-reference-manual-is-missing-the-I2C-chapter/m-p/494701#M30698</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-12-17T23:32:29Z</dc:date>
    </item>
  </channel>
</rss>