<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Serial Communication between two FRDM-KE02Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-Communication-between-two-FRDM-KE02Z/m-p/494623#M30665</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example or advice how to configure the UART interface for the data transfer between two freedomboard?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernadett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Apr 2016 06:58:24 GMT</pubDate>
    <dc:creator>bernadettmarton</dc:creator>
    <dc:date>2016-04-11T06:58:24Z</dc:date>
    <item>
      <title>Serial Communication between two FRDM-KE02Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-Communication-between-two-FRDM-KE02Z/m-p/494623#M30665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example or advice how to configure the UART interface for the data transfer between two freedomboard?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernadett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 06:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-Communication-between-two-FRDM-KE02Z/m-p/494623#M30665</guid>
      <dc:creator>bernadettmarton</dc:creator>
      <dc:date>2016-04-11T06:58:24Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Communication between two FRDM-KE02Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-Communication-between-two-FRDM-KE02Z/m-p/494624#M30666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello bernadett,&lt;/P&gt;&lt;P&gt;There is a UART demo about FRDM-KE02Z in the attachment ,&amp;nbsp; you can refer to it , after download&lt;/P&gt;&lt;P&gt;it , then you can find it at here :&lt;/P&gt;&lt;P&gt;KE02-SC\ke02-sc\src\projects\Uart_demo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the demo information you can refer to the "Readme.txt" :&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The UART1 sends the "Running the Uart_demo project" with polling mode.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;and then enter the interrupt mode.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; First, the UART1 sends the string "hello world" to the hyperterminal;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Second, the UART1 will send the character to Hyperterminal which you entered,&amp;nbsp; and RED led will flicker.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Hope it helps!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 07:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Serial-Communication-between-two-FRDM-KE02Z/m-p/494624#M30666</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-04-11T07:45:59Z</dc:date>
    </item>
  </channel>
</rss>