<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB CDC Driver on USB-KW24D512 problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CDC-Driver-on-USB-KW24D512-problem/m-p/494212#M30620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the function in bsp, USB_Init and CDC_ModuleInit, meanwhile the board is working in PEE mode.&lt;/P&gt;&lt;P&gt;The enumeration completed successfully.&lt;/P&gt;&lt;P&gt;After enumeration, I tried to talk with the board via the minicom in Linux.&lt;/P&gt;&lt;P&gt;But there is not any response when typing in minicom.&lt;/P&gt;&lt;P&gt;The board is able to get SOF interrupt, but there are not TOKEN interrupt received.&lt;/P&gt;&lt;P&gt;Are there any problems here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Mar 2016 08:40:42 GMT</pubDate>
    <dc:creator>luwan</dc:creator>
    <dc:date>2016-03-22T08:40:42Z</dc:date>
    <item>
      <title>USB CDC Driver on USB-KW24D512 problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CDC-Driver-on-USB-KW24D512-problem/m-p/494212#M30620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the function in bsp, USB_Init and CDC_ModuleInit, meanwhile the board is working in PEE mode.&lt;/P&gt;&lt;P&gt;The enumeration completed successfully.&lt;/P&gt;&lt;P&gt;After enumeration, I tried to talk with the board via the minicom in Linux.&lt;/P&gt;&lt;P&gt;But there is not any response when typing in minicom.&lt;/P&gt;&lt;P&gt;The board is able to get SOF interrupt, but there are not TOKEN interrupt received.&lt;/P&gt;&lt;P&gt;Are there any problems here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 08:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CDC-Driver-on-USB-KW24D512-problem/m-p/494212#M30620</guid>
      <dc:creator>luwan</dc:creator>
      <dc:date>2016-03-22T08:40:42Z</dc:date>
    </item>
  </channel>
</rss>