<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMust USB clock source be 48MHz clock on USB-KW24D512?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Must-USB-clock-source-be-48MHz-clock-on-USB-KW24D512/m-p/494171#M30616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Can this 20~25MHz clock after start-up be used for driving USB driver?&lt;/P&gt;&lt;P&gt;If 20~25MHz is not large enough, can we scale the clock to 48MHz via configuring MCG_C4, but still keep running in FEI mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Mar 2016 02:47:39 GMT</pubDate>
    <dc:creator>luwan</dc:creator>
    <dc:date>2016-03-22T02:47:39Z</dc:date>
    <item>
      <title>Must USB clock source be 48MHz clock on USB-KW24D512?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Must-USB-clock-source-be-48MHz-clock-on-USB-KW24D512/m-p/494171#M30616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Can this 20~25MHz clock after start-up be used for driving USB driver?&lt;/P&gt;&lt;P&gt;If 20~25MHz is not large enough, can we scale the clock to 48MHz via configuring MCG_C4, but still keep running in FEI mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 02:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Must-USB-clock-source-be-48MHz-clock-on-USB-KW24D512/m-p/494171#M30616</guid>
      <dc:creator>luwan</dc:creator>
      <dc:date>2016-03-22T02:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: Must USB clock source be 48MHz clock on USB-KW24D512?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Must-USB-clock-source-be-48MHz-clock-on-USB-KW24D512/m-p/494172#M30617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;No, you can not do that. The USB clock should be 48MHz and as I had mentioned that we do not recommend to use FLL to clock the USB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 08:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Must-USB-clock-source-be-48MHz-clock-on-USB-KW24D512/m-p/494172#M30617</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-03-23T08:03:21Z</dc:date>
    </item>
  </channel>
</rss>