<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL02 ISSUES - order code</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-ISSUES-order-code/m-p/493660#M30566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matteo,&lt;/P&gt;&lt;P&gt;We'd like to suggest that you should additional point out the mask set number when you order the KL02 from the distributor.&lt;/P&gt;&lt;P&gt;And website ordering system can guarantee that you can receive the specific version you want.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Apr 2016 03:29:03 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-04-12T03:29:03Z</dc:date>
    <item>
      <title>KL02 ISSUES - order code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-ISSUES-order-code/m-p/493659#M30565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the KL02 Kinetis microcontroller and i've found the "mask set errata" for revision 0N33H (&lt;A href="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_L_0N33H.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_L_0N33H.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt; http://cache.nxp.com/files/32bit/doc/errata/KINETIS_L_0N33H.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt; ).&lt;/P&gt;&lt;P&gt;I verified that the KL02 mounted on my prototipes are 0N33H revision reading the REVID field in the SIM_SDID register. I cannot follow the workaround because in my project the 1.8V Vdd is mandatory.&lt;/P&gt;&lt;P&gt;So i've made the revision number 2 of the project and i've specified to my supplier that the KL02 must be of revision 1N33H following the NXP errata note.&lt;/P&gt;&lt;P&gt;So here is the question. How can i distinguish (and my supplier too) revision 0N33H from revision 1N33H during order time if they both has the same order code? Why use the same code for two different revisions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matteo D.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 08:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-ISSUES-order-code/m-p/493659#M30565</guid>
      <dc:creator>matteodavanzo</dc:creator>
      <dc:date>2016-04-11T08:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 ISSUES - order code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-ISSUES-order-code/m-p/493660#M30566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matteo,&lt;/P&gt;&lt;P&gt;We'd like to suggest that you should additional point out the mask set number when you order the KL02 from the distributor.&lt;/P&gt;&lt;P&gt;And website ordering system can guarantee that you can receive the specific version you want.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Apr 2016 03:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-ISSUES-order-code/m-p/493660#M30566</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-12T03:29:03Z</dc:date>
    </item>
  </channel>
</rss>