<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: USB3.0 and K65</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493404#M30542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K65 product has the Flexbus module.&lt;/P&gt;&lt;P&gt;The chapter 34 of &lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/K65P169M180SF5RMV2.pdf"&gt;K65 reference manual&lt;/A&gt; provides the detailed info.&lt;/P&gt;&lt;P&gt;There is an application note about multiplexing pins between SDRAM and Flexbus on K65.&lt;/P&gt;&lt;P&gt;For more detailed info, please check &lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN5095.pdf"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jan 2016 08:07:09 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-01-18T08:07:09Z</dc:date>
    <item>
      <title>USB3.0 and K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493402#M30540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using K65, external SDRAM, and SD card. Is it possible to connect FT600 to that configuration?&lt;/P&gt;&lt;P&gt;I know that FT600 doesn't have FLEX-BUS. I am also using K65 USB 2.0 port.&lt;/P&gt;&lt;P&gt;This is the last moment customer request to add USB3.0 support (as second USB port).&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;g&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;p.s.&lt;/P&gt;&lt;P&gt;I have seen the discussion:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/382737"&gt;usb3.0 with K80&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 14:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493402#M30540</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-01-15T14:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: USB3.0 and K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493403#M30541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K65 doesn't have FLEXBUS&lt;BR /&gt;FT600 uses 16b FIFO&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;g&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 14:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493403#M30541</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-01-15T14:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB3.0 and K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493404#M30542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K65 product has the Flexbus module.&lt;/P&gt;&lt;P&gt;The chapter 34 of &lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/K65P169M180SF5RMV2.pdf"&gt;K65 reference manual&lt;/A&gt; provides the detailed info.&lt;/P&gt;&lt;P&gt;There is an application note about multiplexing pins between SDRAM and Flexbus on K65.&lt;/P&gt;&lt;P&gt;For more detailed info, please check &lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN5095.pdf"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 08:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493404#M30542</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-01-18T08:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: USB3.0 and K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493405#M30543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;It doesn't have flex memory, but it has the flex bus.&lt;/P&gt;&lt;P&gt;I appreciate your response&lt;/P&gt;&lt;P&gt;g&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 14:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB3-0-and-K65/m-p/493405#M30543</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-01-18T14:13:12Z</dc:date>
    </item>
  </channel>
</rss>