<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックInterfacing K70 and GPRS Modem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-K70-and-GPRS-Modem/m-p/492754#M30448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the K70 tower board and want to have 4g and GPS feature. As per the examples provided by Fresscale, K70 can be interfaced to SIM900 which is a GPRS modem. Is it possible to interface K70 to SIM7250E which is an LTE modem that supports 4G and GPS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks ,&lt;/P&gt;&lt;P&gt;Sneha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2016 11:53:54 GMT</pubDate>
    <dc:creator>snehahegde</dc:creator>
    <dc:date>2016-02-05T11:53:54Z</dc:date>
    <item>
      <title>Interfacing K70 and GPRS Modem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-K70-and-GPRS-Modem/m-p/492754#M30448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the K70 tower board and want to have 4g and GPS feature. As per the examples provided by Fresscale, K70 can be interfaced to SIM900 which is a GPRS modem. Is it possible to interface K70 to SIM7250E which is an LTE modem that supports 4G and GPS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks ,&lt;/P&gt;&lt;P&gt;Sneha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 11:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-K70-and-GPRS-Modem/m-p/492754#M30448</guid>
      <dc:creator>snehahegde</dc:creator>
      <dc:date>2016-02-05T11:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing K70 and GPRS Modem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-K70-and-GPRS-Modem/m-p/492755#M30449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sneha,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K70 is able to connect to GPRS modems which support PPP interface which is the case of SIM900. I don't see the LTE module supports PPP in any of the published specs. If you are sure that it does then you should have no issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case it support PPP you can refer to the document below which shows how to create a PPP connection with an MCU using MQX and Windows. In your case in the other side of the MCU you will have LTE modem instead of Windows.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-106483"&gt;How to Create a PPP Connection with MQX4.2 and Win 7&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 22:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interfacing-K70-and-GPRS-Modem/m-p/492755#M30449</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2016-02-10T22:49:38Z</dc:date>
    </item>
  </channel>
</rss>