<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Capacitors on VDDA and VREFH</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Capacitors-on-VDDA-and-VREFH/m-p/203278#M3041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;They are bypass capacitors. They have different capacitance, ESR and ESL that help to eliminate the noise at different frequencies.&lt;/P&gt;&lt;P&gt;If you put only one, the noise at a frequency range may effects to working of the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can get more information if google with "bypass capacitor combination"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2012 12:40:17 GMT</pubDate>
    <dc:creator>Dekiru</dc:creator>
    <dc:date>2012-02-08T12:40:17Z</dc:date>
    <item>
      <title>Capacitors on VDDA and VREFH</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Capacitors-on-VDDA-and-VREFH/m-p/203277#M3040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see two capacitors for VDDA and two capacitors for VREFH pins on TWR-K60N512. They are both X7R chip capacitors, 100nF and 10nF.&lt;/P&gt;&lt;P&gt;What is the reason to use two of them? Is it sufficient to use a single 100nF X7R capacitor near VDDA and VREFH pins of microcontroller?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2012 00:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Capacitors-on-VDDA-and-VREFH/m-p/203277#M3040</guid>
      <dc:creator>pozz</dc:creator>
      <dc:date>2012-02-07T00:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: Capacitors on VDDA and VREFH</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Capacitors-on-VDDA-and-VREFH/m-p/203278#M3041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;They are bypass capacitors. They have different capacitance, ESR and ESL that help to eliminate the noise at different frequencies.&lt;/P&gt;&lt;P&gt;If you put only one, the noise at a frequency range may effects to working of the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can get more information if google with "bypass capacitor combination"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 12:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Capacitors-on-VDDA-and-VREFH/m-p/203278#M3041</guid>
      <dc:creator>Dekiru</dc:creator>
      <dc:date>2012-02-08T12:40:17Z</dc:date>
    </item>
  </channel>
</rss>