<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL03 time to wait after bandgap buffer is enabled</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-time-to-wait-after-bandgap-buffer-is-enabled/m-p/491312#M30328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin Krause,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, we also don't have the bandgap voltage reference stable time, this time must be very small, but we don't have the precise data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Normally, If customer want to use the bandgap as the ADC input,&amp;nbsp; they can enable the bandgap before the ADC initialization, then the bandgap stable time must be enough.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, please try to enable PMC_REGSC[BGBE] bit before the ADC initialization code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact with me!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Mar 2016 05:57:50 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-03-22T05:57:50Z</dc:date>
    <item>
      <title>KL03 time to wait after bandgap buffer is enabled</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-time-to-wait-after-bandgap-buffer-is-enabled/m-p/491311#M30327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How long do I have to wait after enabling the bandgap buffer on an KL03 MCU before the read ADC value for the bandgap channel is stable? In the datasheet / user manual there is no time specified.&lt;/P&gt;&lt;P&gt;I'm asking, because when I do not wait any time, and just enable the bandgap buffer and then immediately afterwards do an ADC measurement of the bandgap, the ADC value "jumps" at higher MCU temeratures (&amp;gt; 50°C). If I add an delay of about 2 us, between enabling the bandgap buffer and measuring the internal bandgap voltage, the ADC value for the bandgap stops jumping, even at higher MCU temeratures (&amp;gt;80°C). My MCU runs at the 8 MHz internal clock, when I do this measurements, the ADC-Clock runs on ADC asynchronous clock source with ADLPC = 0 and ADHSC = 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I assume, there is a waiting time after enabling the bandgap buffer, before I should do measue the ADC bandgap channel to get stable values. The question is how long should I wait to get stable values over the whole MCU temperature range?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Mar 2016 12:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-time-to-wait-after-bandgap-buffer-is-enabled/m-p/491311#M30327</guid>
      <dc:creator>martinkrause</dc:creator>
      <dc:date>2016-03-21T12:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 time to wait after bandgap buffer is enabled</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-time-to-wait-after-bandgap-buffer-is-enabled/m-p/491312#M30328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin Krause,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, we also don't have the bandgap voltage reference stable time, this time must be very small, but we don't have the precise data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Normally, If customer want to use the bandgap as the ADC input,&amp;nbsp; they can enable the bandgap before the ADC initialization, then the bandgap stable time must be enough.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, please try to enable PMC_REGSC[BGBE] bit before the ADC initialization code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact with me!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 05:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-time-to-wait-after-bandgap-buffer-is-enabled/m-p/491312#M30328</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-03-22T05:57:50Z</dc:date>
    </item>
  </channel>
</rss>