<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKL03 DAC output pin</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489055#M30153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm designing a board with the KL03 which uses the 6-bit DAC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What pin does the voltage appear on?&amp;nbsp; I don't want to use the internal comparator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:mrages@sram.com"&gt;mrages@sram.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Dec 2015 21:27:33 GMT</pubDate>
    <dc:creator>markrages</dc:creator>
    <dc:date>2015-12-16T21:27:33Z</dc:date>
    <item>
      <title>KL03 DAC output pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489055#M30153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm designing a board with the KL03 which uses the 6-bit DAC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What pin does the voltage appear on?&amp;nbsp; I don't want to use the internal comparator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:mrages@sram.com"&gt;mrages@sram.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 21:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489055#M30153</guid>
      <dc:creator>markrages</dc:creator>
      <dc:date>2015-12-16T21:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 DAC output pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489056#M30154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From the datasheet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The 6-bit DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ah well, back to xmega for this project then,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 22:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489056#M30154</guid>
      <dc:creator>markrages</dc:creator>
      <dc:date>2015-12-16T22:02:08Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 DAC output pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489057#M30155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark Rages:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is correct, the 6-bit DAC in KL03 is only internal. Sorry for this inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could look at the KL05 family, which integrates a 12-bit DAC with output pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 23:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin/m-p/489057#M30155</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-12-16T23:35:20Z</dc:date>
    </item>
  </channel>
</rss>