<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K82F Red LED when Running QSPI Program</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-Red-LED-when-Running-QSPI-Program/m-p/488179#M30087</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to a colleague the red LED shining brightly (and not flickering) means the device is being held in a reset state.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 15:14:15 GMT</pubDate>
    <dc:creator>jozefl</dc:creator>
    <dc:date>2016-04-28T15:14:15Z</dc:date>
    <item>
      <title>FRDM-K82F Red LED when Running QSPI Program</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-Red-LED-when-Running-QSPI-Program/m-p/488178#M30086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've built a program with the QSPI linker script and flashed it to the board following the standard procedure. However when I plug the USB cable into the openSDA port then a red LED (D2) instantly lights up. Pressing SW1 does not make it go away.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The program also does not run properly. I've noticed that with QSPI programs that work properly this LED does not light up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What does this LED mean? Perhaps the program has been flashed incorrectly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've looked through the K80-sub family ref manual for some information about this LED but couldn't find anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 13:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-Red-LED-when-Running-QSPI-Program/m-p/488178#M30086</guid>
      <dc:creator>jozefl</dc:creator>
      <dc:date>2016-04-28T13:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F Red LED when Running QSPI Program</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-Red-LED-when-Running-QSPI-Program/m-p/488179#M30087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to a colleague the red LED shining brightly (and not flickering) means the device is being held in a reset state.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 15:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-Red-LED-when-Running-QSPI-Program/m-p/488179#M30087</guid>
      <dc:creator>jozefl</dc:creator>
      <dc:date>2016-04-28T15:14:15Z</dc:date>
    </item>
  </channel>
</rss>