<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCreating External Flash Algorithm for CW10.2 and Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Creating-External-Flash-Algorithm-for-CW10-2-and-Kinetis/m-p/202851#M3008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a document (AN3859) which describes how to create external flash algorithm for CW10 and ColdFire. I need to create such algorithm for Kinetis (we are using external flash).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN3859 says that&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- I need the sources of the Flash Tool Kit (FTK). But within CW10.2 package there are only sources for Coldfire.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Where can I find FTK sources for Kinetis CPUs?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- I need the specification how CW10 passes the flashing parameters to the flash algorithm. AN859 describes it for the ColdFire CPUs (on Coldfire CPUs CW10 passes a pointer to the parameters within the D7 register). How is that done on Kinetis CPUs?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Johann&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2012 18:44:23 GMT</pubDate>
    <dc:creator>Icenine</dc:creator>
    <dc:date>2012-02-03T18:44:23Z</dc:date>
    <item>
      <title>Creating External Flash Algorithm for CW10.2 and Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Creating-External-Flash-Algorithm-for-CW10-2-and-Kinetis/m-p/202851#M3008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found a document (AN3859) which describes how to create external flash algorithm for CW10 and ColdFire. I need to create such algorithm for Kinetis (we are using external flash).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;AN3859 says that&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- I need the sources of the Flash Tool Kit (FTK). But within CW10.2 package there are only sources for Coldfire.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Where can I find FTK sources for Kinetis CPUs?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- I need the specification how CW10 passes the flashing parameters to the flash algorithm. AN859 describes it for the ColdFire CPUs (on Coldfire CPUs CW10 passes a pointer to the parameters within the D7 register). How is that done on Kinetis CPUs?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Johann&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2012 18:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Creating-External-Flash-Algorithm-for-CW10-2-and-Kinetis/m-p/202851#M3008</guid>
      <dc:creator>Icenine</dc:creator>
      <dc:date>2012-02-03T18:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: Creating External Flash Algorithm for CW10.2 and Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Creating-External-Flash-Algorithm-for-CW10-2-and-Kinetis/m-p/202852#M3009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need the sources for the Kinetis FTK as well! I'm assuming that the setup for the flexbus can be included as part of the flash algorithm.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2012 05:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Creating-External-Flash-Algorithm-for-CW10-2-and-Kinetis/m-p/202852#M3009</guid>
      <dc:creator>ERussell</dc:creator>
      <dc:date>2012-02-04T05:40:43Z</dc:date>
    </item>
  </channel>
</rss>