<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KBI interface with ke02</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485676#M29810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;That was the gate clocking issue. Now the issue is that I cannot enable interrupt on both pins. When Kbi1_PE is 0x90(both pin selected in pin enable) only the ptd4 pin triggers the input. Ptd7 does not. When kbi1_PE is 0x80(only ptd7 selected), ptd7 works fine. Ptd4 is the output of a logical device, ptd7 is mechanical switch pulled up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Apr 2016 11:42:11 GMT</pubDate>
    <dc:creator>surajka</dc:creator>
    <dc:date>2016-04-29T11:42:11Z</dc:date>
    <item>
      <title>KBI interface with ke02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485675#M29809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working with kbi but not getting the isr working. I have ptd4 and ptd7 connected to two switches, the first one switches to vcc and the other one switch to ground(pull up resistors done). I have attached my code&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337355"&gt;TEST_KBI.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 12:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485675#M29809</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-28T12:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: KBI interface with ke02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485676#M29810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;That was the gate clocking issue. Now the issue is that I cannot enable interrupt on both pins. When Kbi1_PE is 0x90(both pin selected in pin enable) only the ptd4 pin triggers the input. Ptd7 does not. When kbi1_PE is 0x80(only ptd7 selected), ptd7 works fine. Ptd4 is the output of a logical device, ptd7 is mechanical switch pulled up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 11:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485676#M29810</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-29T11:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: KBI interface with ke02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485677#M29811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The kbi_es register was 0x00 earlier. I changed it to 0x14 and its working fine now. But I am not able to reverse the edge trigger polarity. Due to this, interrupt occurs two times back to back. May be keypad bouncing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 11:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-interface-with-ke02/m-p/485677#M29811</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-29T11:56:26Z</dc:date>
    </item>
  </channel>
</rss>