<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Treat MKW24D512VHA5 as a SPI master</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485593#M29805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Earl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw below info on page 17, MKW2xDxxx.pdf, Rev. 1, 11/2013.&lt;/P&gt;&lt;P&gt;The MKW2x SiP uses a SPI interface allowing the MCU to communicate with the radio's&lt;/P&gt;&lt;P&gt;register set and packet buffer. The SPI is a slave-only interface; the MCU must drive&lt;/P&gt;&lt;P&gt;R_SSEL_B, R_SCLK and R_MOSI, ..., etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can a MKW24D512VHA5 be SPI master to connect to SPI slave (e.g. a temperature sensor)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Feb 2016 16:13:20 GMT</pubDate>
    <dc:creator>diaskuo</dc:creator>
    <dc:date>2016-02-08T16:13:20Z</dc:date>
    <item>
      <title>Treat MKW24D512VHA5 as a SPI master</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485591#M29803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can MKW24D512VHA5 treat as a SPI master device to connect with a sensor device (SPI slave)?&lt;/P&gt;&lt;P&gt;Would you please guide me to setup the SPI master?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 02:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485591#M29803</guid>
      <dc:creator>diaskuo</dc:creator>
      <dc:date>2016-02-04T02:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: Treat MKW24D512VHA5 as a SPI master</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485592#M29804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dias,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using some specific software? If you aren't, I recommend you to take a look into the &lt;A href="http://nxp.com/ksdk"&gt;Kinetis SDK&lt;/A&gt;​, once you have installed the SDK please go to the folder &lt;STRONG&gt;C:\Freescale\KSDK_1.3.0\examples\twrkw24d512\driver_examples\dspi\dspi_non_blocking\master&lt;/STRONG&gt; and open the project. This example code will help you enabling what you are asking for.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a BeeKit generated project, it already includes some functions to use the SPI instance which includes your MCU. You can find them in &lt;STRONG&gt;PLM/Source/SPI&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60618i4B443CFEFF232F1F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you need any additional direction and if this is useful for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 21:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485592#M29804</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2016-02-05T21:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: Treat MKW24D512VHA5 as a SPI master</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485593#M29805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Earl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw below info on page 17, MKW2xDxxx.pdf, Rev. 1, 11/2013.&lt;/P&gt;&lt;P&gt;The MKW2x SiP uses a SPI interface allowing the MCU to communicate with the radio's&lt;/P&gt;&lt;P&gt;register set and packet buffer. The SPI is a slave-only interface; the MCU must drive&lt;/P&gt;&lt;P&gt;R_SSEL_B, R_SCLK and R_MOSI, ..., etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can a MKW24D512VHA5 be SPI master to connect to SPI slave (e.g. a temperature sensor)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 16:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485593#M29805</guid>
      <dc:creator>diaskuo</dc:creator>
      <dc:date>2016-02-08T16:13:20Z</dc:date>
    </item>
    <item>
      <title>Re: Treat MKW24D512VHA5 as a SPI master</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485594#M29806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dias,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MKW2xD devices include one additional SPI instance additionally to the one used to control the internal radio. The section you are referring makes reference to the radio's SPI instance but the another instance can works either as master or slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 16:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Treat-MKW24D512VHA5-as-a-SPI-master/m-p/485594#M29806</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2016-02-08T16:28:22Z</dc:date>
    </item>
  </channel>
</rss>