<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: PK60F120M Reset pin oscillating</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202188#M2980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, Kevin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is blank. My problem is that I cannot programme it.. I should say I cannot not even establish connection with it. I am using Multilink FX via CodeWarrior. I captured the TCK and TDI signals from Multilink but do not see TDO signal from Kinetis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which programming tool are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2012 09:39:25 GMT</pubDate>
    <dc:creator>keithtang</dc:creator>
    <dc:date>2012-09-27T09:39:25Z</dc:date>
    <item>
      <title>PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202186#M2978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thought I should start a new topic instead of replying to member's post to get attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having problem with my PK60F120M (mask code 1N96B) chips. They are oscillating at 1.45 KHz (sawtooth wave swings from 0 V to 1.6V). I tried all suggestions given by other members, such as holding the reset pin while powering up, reduce the power up slew rate, pull the EZ_CS pin high, etc without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have sent direct request to Freescale technical support with no answer after 48 hours. The FAE can't give positive suggestion too. We are basically left in the dark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need the solution urgently, please can someone help. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 09:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202186#M2978</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-09-27T09:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202187#M2979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've also had a problem with the RESET_B pin on my PK60FN1M0VLQ12 device however my FAE put it down to it being a blank device. Once programmed, the signal stops oscillating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm presuming that yours still does it even when programmed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For reference, my device has the same mask code as yours.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 09:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202187#M2979</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2012-09-27T09:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202188#M2980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply, Kevin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes it is blank. My problem is that I cannot programme it.. I should say I cannot not even establish connection with it. I am using Multilink FX via CodeWarrior. I captured the TCK and TDI signals from Multilink but do not see TDO signal from Kinetis.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which programming tool are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 09:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202188#M2980</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-09-27T09:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202189#M2981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using IAR EWARM with a Segger J-Link however I had to resort to using the Segger J-Flash software to program it as the version of IAR I had installed wouldn't let me program the device. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version of the JTAG header are you using? I'm using the 9 pin version and it is now working perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 09:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202189#M2981</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2012-09-27T09:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202190#M2982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yeah. I have read about J-Link is able to solve the problem with the latest firmware, although I wonder how they do it. I have never used J-Link before and was hesitating if i should get a J-Link EDU (instead of J-Link, as it is a bit pricy) to try. Do you think J-Link EDU does the same job?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't get you. What do you mean by "version of JTAG header"?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 09:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202190#M2982</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-09-27T09:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202191#M2983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was originally using an IAR I-jet however I had lots of problems trying to program the device with it. I now use a J-Link EDU to program and debug the chip and it works perfectly. I know that the Segger website has a comparison of the various J-Link flavours but from my perspective, the EDU version has all the features I need. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By version of header, I was referring to whether you were using a MIPI-20 or MIPI-10 connector. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 10:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202191#M2983</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2012-09-27T10:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202192#M2984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK I think I will get the EDU then. Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, I am using MIPI-20 connector.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 10:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202192#M2984</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-09-27T10:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202193#M2985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On a blank device, all of the flash memory sits at the erased state 0xFF (except address 0x0000_040C FSEC which is 0xFE).&lt;/P&gt;&lt;P&gt;You fit the device to your board, and apply power. The core goes to 0x0000_0000 to fetch the initial stack pointer and 0x0000_0004 to fetch the reset vector. Both of these read 0xFFFF-FFFF and so these are illegal addresses. The chip ultimately resets, and starts all over again.&lt;/P&gt;&lt;P&gt;The symptom is that the reset line oscillates as the chip runs (reset high) then resets (reset low). It's not unexpected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 16:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202193#M2985</guid>
      <dc:creator>UK_CF_FAE</dc:creator>
      <dc:date>2012-09-27T16:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202194#M2986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the info, Mark.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2012 04:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202194#M2986</guid>
      <dc:creator>keithtang</dc:creator>
      <dc:date>2012-09-28T04:44:46Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202195#M2987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark,&lt;/P&gt;&lt;P&gt;We are seeing the same issue on a K70 target design (reset is inactive for ~2us, then is active for ~50us, repeating).&amp;nbsp; When we connect an IAR I-Jet, the IAR debugger is unable to complete the reset sequence to download code to the part.&amp;nbsp; How does one get the part initially programmed?&lt;/P&gt;&lt;P&gt;Our JTAG interface (on our target board) is identical to the TWR-K70F120M.&lt;/P&gt;&lt;P&gt;Thoughts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2013 21:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202195#M2987</guid>
      <dc:creator>wiilliam_powell</dc:creator>
      <dc:date>2013-02-27T21:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202196#M2988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;First thing you have to do is get the Jlink command line utility. If you have and IAR installation then in the installation path \Embedded Workbench 6.4_2\arm\bin&amp;nbsp; you will find the Jlink.exe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now power your board with the J-link connected. Press the reset pin, holding the reset pin down power cycle your board and with the reset pin held low you run the Jlink.exe. If your debug interface is correct on the command window you will see the message that J-link communication was established with the controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can release the reset pin now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the command prompt you type "Unlock Kineits". this will un secure the controller and now you should be able to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After this close the Jlink window and start again to see that it gives the JTAG communication okay messages or prompts any error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now your reset should not toggle any more.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2013 07:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202196#M2988</guid>
      <dc:creator>deepakrana</dc:creator>
      <dc:date>2013-02-28T07:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: PK60F120M Reset pin oscillating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202197#M2989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Deepak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.  We will give this a try.  We were using an I-Jet and having the problem connecting.  This morning, we tried connecting with a J-Link and were able to get the unit programmed.  Looks like there might be some difference between the I-Jet and J-Link and how the debuggers take control of the micro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;William (Bill) Powell  |  Principal Software Engineer&lt;/P&gt;&lt;P&gt;Indesign, LLC | •: 8225 E 56th Street, Indianapolis, IN 46216 | • Office: 317-377-5439 | 7 Fax: 317-377-5455&lt;/P&gt;&lt;P&gt;&lt;A href="www.Indesign-LLC.com&amp;lt;http://www.indesign-llc.com/&amp;gt;" target="test_blank"&gt;www.Indesign-LLC.com&amp;lt;http://www.indesign-llc.com/&amp;gt;&lt;/A&gt;;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2013 15:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK60F120M-Reset-pin-oscillating/m-p/202197#M2989</guid>
      <dc:creator>wiilliam_powell</dc:creator>
      <dc:date>2013-02-28T15:12:17Z</dc:date>
    </item>
  </channel>
</rss>