<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Interrupt CAN with k10 cortex M4F and freertos v8.2.2 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485503#M29799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Slah，&lt;/P&gt;&lt;P&gt;Actually there's no difference to create a interrupt function no matter integrate with the FreeRTOS or just baremetal.&lt;/P&gt;&lt;P&gt;I'd highly recommend that you should check the interrupt function should be assigned to the vector table correctly.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 08:02:59 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-01-13T08:02:59Z</dc:date>
    <item>
      <title>Interrupt CAN with k10 cortex M4F and freertos v8.2.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485502#M29798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;I am developing&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a program on&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;K10&lt;/SPAN&gt; &lt;SPAN class="hps atn"&gt;Cortex-&lt;/SPAN&gt;M4F &lt;SPAN class="hps"&gt;that uses the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;CAN bus interrupt&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;but I do&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;not get any&lt;/SPAN&gt; &lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;CAN hardware &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;interruption&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;FreeRTOS, &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;However&lt;/SPAN&gt;&lt;SPAN&gt;, the messages&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;circulating&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;on the bus&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;BR /&gt;&lt;SPAN class="hps"&gt;For information, I&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;used&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;processor&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;expert&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and authorize&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;NMI&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;interrupt&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;interrupt&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;service to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the CAN bus.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="hps"&gt;I wanted to know&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;if&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;FreeRTOS&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;can block&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;material&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;interruptions?&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;what to do to allow&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;hardware&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;interrupt&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;FreeRTOS&lt;/SPAN&gt;?&lt;BR /&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;Thank you&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 14:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485502#M29798</guid>
      <dc:creator>achourislaheddi</dc:creator>
      <dc:date>2016-01-12T14:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt CAN with k10 cortex M4F and freertos v8.2.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485503#M29799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Slah，&lt;/P&gt;&lt;P&gt;Actually there's no difference to create a interrupt function no matter integrate with the FreeRTOS or just baremetal.&lt;/P&gt;&lt;P&gt;I'd highly recommend that you should check the interrupt function should be assigned to the vector table correctly.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 08:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485503#M29799</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-13T08:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt CAN with k10 cortex M4F and freertos v8.2.2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485504#M29800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First be sure the problem is related to FreeRTOS by trying to use the interrupt in a dummy app that doesn't use FreeRTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you find the interrupt works after the FreeRTOS scheduler has been started, but not before?&amp;nbsp; if so, see number 3 on the following FAQ page: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freertos.org/FAQHelp.html" rel="nofollow"&gt;http://www.freertos.org/FAQHelp.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 08:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Interrupt-CAN-with-k10-cortex-M4F-and-freertos-v8-2-2/m-p/485504#M29800</guid>
      <dc:creator>FreeRTOS_org</dc:creator>
      <dc:date>2016-01-13T08:27:35Z</dc:date>
    </item>
  </channel>
</rss>