<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKEA64 get flash size</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA64-get-flash-size/m-p/484880#M29727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the KEA64 family and I am wondering if it is possible to get the flash size of the MCU at runtime?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Dec 2015 14:26:14 GMT</pubDate>
    <dc:creator>philippetrudel</dc:creator>
    <dc:date>2015-12-15T14:26:14Z</dc:date>
    <item>
      <title>KEA64 get flash size</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA64-get-flash-size/m-p/484880#M29727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the KEA64 family and I am wondering if it is possible to get the flash size of the MCU at runtime?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 14:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA64-get-flash-size/m-p/484880#M29727</guid>
      <dc:creator>philippetrudel</dc:creator>
      <dc:date>2015-12-15T14:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: KEA64 get flash size</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA64-get-flash-size/m-p/484881#M29728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no register containing the Flash size but you can test it as follows:&lt;/P&gt;&lt;P&gt;- try to read a byte/word from Flash at 0xfff0 - if it causes a hard fault (which you need to handle appropriately) it is &amp;lt; 64k, otherwise it is 64k&lt;/P&gt;&lt;P&gt;- repeat at 0x7ff0 - if it also fauts it is 16k or else it is 32k&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 15:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA64-get-flash-size/m-p/484881#M29728</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-12-15T15:58:23Z</dc:date>
    </item>
  </channel>
</rss>