<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FlexBus for Intel 8080 parallel bus transfers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484571#M29708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks! This goes in the right direction. The speciality is that on Intel 8080 you have separate read and write signals (unlike on Motorola 6800 where a single R/W signal is used).&lt;/P&gt;&lt;P&gt;I don't know if anybody has ever worked on a solution with FlexBus to interface it to Intel 8080 bus with or without external logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Dec 2015 11:35:08 GMT</pubDate>
    <dc:creator>guenter_loettrich</dc:creator>
    <dc:date>2015-12-17T11:35:08Z</dc:date>
    <item>
      <title>FlexBus for Intel 8080 parallel bus transfers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484569#M29706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is somebody aware of an example code and circuit diagram that uses FlexBus (on K22) for emulating the Intel 8080 parallel bus implementation (separate Read and Write signals)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 11:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484569#M29706</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2015-12-15T11:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus for Intel 8080 parallel bus transfers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484570#M29707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guenter,&lt;/P&gt;&lt;P&gt;Please check the attachment.&lt;/P&gt;&lt;P&gt;The attachment is a FlexBus_LCD demo, the K22 control the LCD by using the Flexbus module.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31009i5ECF340709D0B166/image-size/large?v=v2&amp;amp;px=999" title="2015-12-17_10-53-47.jpg" alt="2015-12-17_10-53-47.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 02:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484570#M29707</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-12-17T02:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus for Intel 8080 parallel bus transfers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484571#M29708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks! This goes in the right direction. The speciality is that on Intel 8080 you have separate read and write signals (unlike on Motorola 6800 where a single R/W signal is used).&lt;/P&gt;&lt;P&gt;I don't know if anybody has ever worked on a solution with FlexBus to interface it to Intel 8080 bus with or without external logic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 11:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-for-Intel-8080-parallel-bus-transfers/m-p/484571#M29708</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2015-12-17T11:35:08Z</dc:date>
    </item>
  </channel>
</rss>