<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Code Warrior Breakpoint</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Breakpoint/m-p/202057#M2970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;when i want to run the code in debug mode from a Breakpoint, the code&lt;/P&gt;&lt;P&gt;stays at the breakpoint. I have to delete the breakpoint first.&lt;/P&gt;&lt;P&gt;Than I can run the code. When I do not delete the breakpoint the code jumps always to the old&lt;/P&gt;&lt;P&gt;breakpoint.&lt;/P&gt;&lt;P&gt;What can I do to run the code after a breakpoint. I do not want to delete the breakpoint.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the CW10.1. My target is aTWR-k60N512 Tower.&lt;/P&gt;&lt;P&gt;Launch configuration:&lt;/P&gt;&lt;P&gt;TWR_K60_MK60512VMD100_INTERNAL_FLASH_PnE U-MultiLink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for help&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Feb 2012 16:04:06 GMT</pubDate>
    <dc:creator>Thommi_Tulpe</dc:creator>
    <dc:date>2012-02-01T16:04:06Z</dc:date>
    <item>
      <title>Code Warrior Breakpoint</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Breakpoint/m-p/202057#M2970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;when i want to run the code in debug mode from a Breakpoint, the code&lt;/P&gt;&lt;P&gt;stays at the breakpoint. I have to delete the breakpoint first.&lt;/P&gt;&lt;P&gt;Than I can run the code. When I do not delete the breakpoint the code jumps always to the old&lt;/P&gt;&lt;P&gt;breakpoint.&lt;/P&gt;&lt;P&gt;What can I do to run the code after a breakpoint. I do not want to delete the breakpoint.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the CW10.1. My target is aTWR-k60N512 Tower.&lt;/P&gt;&lt;P&gt;Launch configuration:&lt;/P&gt;&lt;P&gt;TWR_K60_MK60512VMD100_INTERNAL_FLASH_PnE U-MultiLink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for help&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2012 16:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Breakpoint/m-p/202057#M2970</guid>
      <dc:creator>Thommi_Tulpe</dc:creator>
      <dc:date>2012-02-01T16:04:06Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior Breakpoint</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Breakpoint/m-p/202058#M2971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that what happens in such cases is that the code is interrupted by pending interrupts when it starts running after a break point, services that interrupt and then stops back at the original break-point again after it returns.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check in the debugger settings to see whether there are options to automatically disable interrupts when breakpoints are hit and then to let it automatically step once before enabling interrupts when running again (or similar).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2012 20:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Code-Warrior-Breakpoint/m-p/202058#M2971</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2012-02-01T20:39:28Z</dc:date>
    </item>
  </channel>
</rss>