<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFTM and timer sample code for Kinetis SDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-and-timer-sample-code-for-Kinetis-SDK/m-p/483839#M29657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any sample applications to use the FTM module for other functionality like interrupt generation, input capture, output compare and external clock inputs? The only demo included in Kinetis SDK v2.0 is a very limited PWM application which doesn't help much with developing other timer applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is FTM the right module to use for generating accurate delays in applications. Should I be looking at another timing module for this purpose (Sleep mode and energy consumption are not my current focus)? Which Kinetis timer system is preferred for use as the core of an RTOS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Platform: I'm using the bare bones SDK with ARM GCC embedded from launchpad on OSX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 May 2016 20:17:59 GMT</pubDate>
    <dc:creator>adongare</dc:creator>
    <dc:date>2016-05-18T20:17:59Z</dc:date>
    <item>
      <title>FTM and timer sample code for Kinetis SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-and-timer-sample-code-for-Kinetis-SDK/m-p/483839#M29657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any sample applications to use the FTM module for other functionality like interrupt generation, input capture, output compare and external clock inputs? The only demo included in Kinetis SDK v2.0 is a very limited PWM application which doesn't help much with developing other timer applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is FTM the right module to use for generating accurate delays in applications. Should I be looking at another timing module for this purpose (Sleep mode and energy consumption are not my current focus)? Which Kinetis timer system is preferred for use as the core of an RTOS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Platform: I'm using the bare bones SDK with ARM GCC embedded from launchpad on OSX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 May 2016 20:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-and-timer-sample-code-for-Kinetis-SDK/m-p/483839#M29657</guid>
      <dc:creator>adongare</dc:creator>
      <dc:date>2016-05-18T20:17:59Z</dc:date>
    </item>
  </channel>
</rss>