<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Urgent: Need help on Hard Fault in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483837#M29655</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a clock that needs turned on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some peripherals generate a hard fault if they are accessed without their clock running, some don't.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I find that inconstancy annoying.&amp;nbsp; Just as annoying it is not documented in the Reference Manual which is which.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Dec 2015 13:52:33 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2015-12-15T13:52:33Z</dc:date>
    <item>
      <title>Urgent: Need help on Hard Fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483836#M29654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've read something about Hard Faults so far and I'm also using a Hard Fault Handler on my KEA128.&lt;/P&gt;&lt;P&gt;However I can't find the reason what is going wrong here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the line of C code resulting in a Hard Fault:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;FTM2_MODE = (FTM_MODE_FAULTM(0x00) | FTM_MODE_WPDIS_MASK);&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I can debug this code in Disassembly View:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31150i9DF41C7E4E0553F9/image-size/large?v=v2&amp;amp;px=999" title="disassembly.PNG" alt="disassembly.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Actually I'm getting the Hard Fault directly on the first assembly instruction, but before it happend only on the 3rd instruction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any hints? Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 09:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483836#M29654</guid>
      <dc:creator>0815</dc:creator>
      <dc:date>2015-12-15T09:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent: Need help on Hard Fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483837#M29655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a clock that needs turned on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some peripherals generate a hard fault if they are accessed without their clock running, some don't.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I find that inconstancy annoying.&amp;nbsp; Just as annoying it is not documented in the Reference Manual which is which.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 13:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483837#M29655</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2015-12-15T13:52:33Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent: Need help on Hard Fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483838#M29656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are right!&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;SIM_SCGC |= SIM_SCGC_FTM2_MASK;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This does the magic.&lt;/P&gt;&lt;P&gt;Thank you, very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 14:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Urgent-Need-help-on-Hard-Fault/m-p/483838#M29656</guid>
      <dc:creator>0815</dc:creator>
      <dc:date>2015-12-15T14:10:40Z</dc:date>
    </item>
  </channel>
</rss>