<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-K22f recovery</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483091#M29552</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello eric netherland:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try connecting the board in &lt;STRONG&gt;BOOTLOADER&lt;/STRONG&gt; mode (hold reset and then connect the USB cable). If the board enumerates as BOOTLOADER then you should be able to load the correct &lt;STRONG&gt;v2.1&lt;/STRONG&gt; interface binary (J-link or P&amp;amp;E) as adviced in the next documents:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101790"&gt;FRDM-K22F: Debugging with Segger J-Link OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101792"&gt;FRDM-K22F: Debugging with P&amp;amp;amp;E OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the board does not enumerate then I think that the OpenSDA bootloader firmware was corrupted when you loaded a wrong binary. In such case you would need an external tool (e.g. P&amp;amp;E Multilink or Segger J-Link) to reprogram the K20 MCU. Attached is an S-Record file for the FRDM-K22F OpenSDA bootloader.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Mar 2016 02:48:07 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-03-18T02:48:07Z</dc:date>
    <item>
      <title>FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483090#M29551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While attempting to update my FRDM-k22f to OpenSDAv2.1 something went wrong.&lt;/P&gt;&lt;P&gt;Following these steps which I have done before with no problems: &lt;A href="https://community.nxp.com/docs/DOC-101790"&gt;FRDM-K22F: Debugging with Segger J-Link OpenSDAv2.1 Firmware&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Enumerating to the Bootloader worked OK but I got an error while copying the .bin file to the device that complained the file was too big. After that all the lights went out and nothing responds. Bricked?&lt;/P&gt;&lt;P&gt;How can I flash back to default?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2016 03:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483090#M29551</guid>
      <dc:creator>ericnetherland</dc:creator>
      <dc:date>2016-03-17T03:33:11Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483091#M29552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello eric netherland:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please try connecting the board in &lt;STRONG&gt;BOOTLOADER&lt;/STRONG&gt; mode (hold reset and then connect the USB cable). If the board enumerates as BOOTLOADER then you should be able to load the correct &lt;STRONG&gt;v2.1&lt;/STRONG&gt; interface binary (J-link or P&amp;amp;E) as adviced in the next documents:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101790"&gt;FRDM-K22F: Debugging with Segger J-Link OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101792"&gt;FRDM-K22F: Debugging with P&amp;amp;amp;E OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the board does not enumerate then I think that the OpenSDA bootloader firmware was corrupted when you loaded a wrong binary. In such case you would need an external tool (e.g. P&amp;amp;E Multilink or Segger J-Link) to reprogram the K20 MCU. Attached is an S-Record file for the FRDM-K22F OpenSDA bootloader.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 02:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483091#M29552</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-18T02:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483092#M29553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Fortunately I have a P&amp;amp;E micro Multilink. If I get a micro 10-pin cable I can try using JTAG to flash it back to life.&lt;/P&gt;&lt;P&gt;Example: &lt;A href="http://mcuoneclipse.com/2015/05/11/debugging-the-frdm-k64f-with-pe-multilink/" title="http://mcuoneclipse.com/2015/05/11/debugging-the-frdm-k64f-with-pe-multilink/"&gt;Debugging the FRDM-K64F with P&amp;amp;E Multilink | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Is there a another link you can recommend for loading the binary in your attachment or do I simply set it up and "flash from file"?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 18:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483092#M29553</guid>
      <dc:creator>ericnetherland</dc:creator>
      <dc:date>2016-03-18T18:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483093#M29554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just set up a connection depending on your programming software and load the binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:smileyalert: Pay attention that the board has 2 programming headers (&lt;STRONG&gt;J11&lt;/STRONG&gt; and &lt;STRONG&gt;J12&lt;/STRONG&gt;). The file I shared is to be loaded in the K20 MCU of the &lt;STRONG&gt;FRDM-K22F&lt;/STRONG&gt; board, so you have to use the &lt;STRONG&gt;J12&lt;/STRONG&gt; header.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 20:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483093#M29554</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-18T20:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483094#M29555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Once I got the micro 10-pin cable I could flash and debug my elf files fine with the P&amp;amp;E JTAG header (j11).&lt;/P&gt;&lt;P&gt;So I'm back in business but without using the USB port. &lt;/P&gt;&lt;P&gt;I tried flashing the file you attached on the J12 header but that didn't work with P&amp;amp;E so I don't have the bootloader back yet.&lt;/P&gt;&lt;P&gt;Does this link describe the process to reload the bootloader into the K20?: &lt;A href="http://mcuoneclipse.com/2014/11/10/recovering-the-frdm-k64f-bootloader-or-cloning-the-program-of-a-microcontroller/" title="http://mcuoneclipse.com/2014/11/10/recovering-the-frdm-k64f-bootloader-or-cloning-the-program-of-a-microcontroller/"&gt;Recovering the FRDM-K64F Bootloader, or: Cloning the Program of a Microcontroller | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Mar 2016 00:43:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483094#M29555</guid>
      <dc:creator>ericnetherland</dc:creator>
      <dc:date>2016-03-19T00:43:55Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483095#M29556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, indeed that link describes what you need to do, but for a FRDM-K22F, which has a &lt;STRONG&gt;v2.1&lt;/STRONG&gt; OpenSDA bootloader, while FRDM-K64F has the &lt;STRONG&gt;v2.0&lt;/STRONG&gt; OpenSDA. Details here: &lt;A href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Mar 2016 02:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483095#M29556</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-19T02:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483096#M29557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to recover v2.1 OpenSDA bootloader on K20 through J12 from another FRDM-K22F?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Sergey.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 12:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483096#M29557</guid>
      <dc:creator>sergeysokolov</dc:creator>
      <dc:date>2016-06-30T12:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483097#M29558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sergey,&lt;/P&gt;&lt;P&gt;have a look at &lt;A href="https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/" title="https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/"&gt;https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;It shows for FRDM-K64F, but applies to FRDM-K22F too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 15:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483097#M29558</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-06-30T15:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22f recovery</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483098#M29559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;May I ask another question related to the issue.&lt;/P&gt;&lt;P&gt;Current status is: Mbed bootloader is overwritten by SeOpenSDA V2.1 Bootloader, after which no enumeration.&lt;/P&gt;&lt;P&gt;The reason why I did it was Mbed's open SDAv2.1 CMSIS-DAP&amp;nbsp; did not support my target MK22FN128VDC10 when I tried to debug from KDSv.3.2.&lt;/P&gt;&lt;P&gt;Question - is the issue known and only solution for MK22FN128VDC10 debugging is switch to Segger Jlink?&lt;/P&gt;&lt;P&gt;Thank you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 07:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22f-recovery/m-p/483098#M29559</guid>
      <dc:creator>sergeysokolov</dc:creator>
      <dc:date>2016-07-01T07:46:50Z</dc:date>
    </item>
  </channel>
</rss>