<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: blhost in NXP_Kinetis_Bootloader_2_0_0</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483051#M29549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sean,&lt;/P&gt;&lt;P&gt;I'm afraid of the kind of approach can't make it.&lt;/P&gt;&lt;P&gt;As Blhost send or receive the command to the deceive only through the UART serial interface, it needs the some kind of 'briage' likes the BusPal.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 May 2016 09:18:40 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-05-19T09:18:40Z</dc:date>
    <item>
      <title>blhost in NXP_Kinetis_Bootloader_2_0_0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483050#M29548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BusPal acts as a bus translator with an established connection with blhost over UART and with the target device over I2C, SPI, or CAN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now my host is linux system and want blhost to support I2C interface to transfer data directly to target without BusPal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you help to provide I2C sample driver code for linux?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean Wu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 04:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483050#M29548</guid>
      <dc:creator>seanwu</dc:creator>
      <dc:date>2016-05-19T04:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: blhost in NXP_Kinetis_Bootloader_2_0_0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483051#M29549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sean,&lt;/P&gt;&lt;P&gt;I'm afraid of the kind of approach can't make it.&lt;/P&gt;&lt;P&gt;As Blhost send or receive the command to the deceive only through the UART serial interface, it needs the some kind of 'briage' likes the BusPal.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 May 2016 09:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483051#M29549</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-05-19T09:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: blhost in NXP_Kinetis_Bootloader_2_0_0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483052#M29550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to modify the make file to build blhost for only UART interface not USB in NXP_Kinetis_Bootloader_2_0_0. Espcially we need to get rid of udev.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 18:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/blhost-in-NXP-Kinetis-Bootloader-2-0-0/m-p/483052#M29550</guid>
      <dc:creator>sensenthuran</dc:creator>
      <dc:date>2016-08-10T18:59:18Z</dc:date>
    </item>
  </channel>
</rss>