<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCan the NMI be used to generate an interrupt while running?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-the-NMI-be-used-to-generate-an-interrupt-while-running/m-p/482902#M29529</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to be able to generate an NMI (Non-Maskable Interrupt) while the processor is running (KL17).&amp;nbsp; The design is to connect it to an external low power detection IC to trigger when the external power is dropping below a threshold.&amp;nbsp; We need this interrupt to save some state information to non-volatile memory before the power drops off completely.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Most of the documentation on the Kinetis systems and the KL17 specifically refers to the NMI as being triggered from the system reset.&amp;nbsp; Is this the only way this interrupt will be triggered or can it be used while the processor is running?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Apr 2016 14:07:32 GMT</pubDate>
    <dc:creator>jmaranhao1</dc:creator>
    <dc:date>2016-04-27T14:07:32Z</dc:date>
    <item>
      <title>Can the NMI be used to generate an interrupt while running?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-the-NMI-be-used-to-generate-an-interrupt-while-running/m-p/482902#M29529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to be able to generate an NMI (Non-Maskable Interrupt) while the processor is running (KL17).&amp;nbsp; The design is to connect it to an external low power detection IC to trigger when the external power is dropping below a threshold.&amp;nbsp; We need this interrupt to save some state information to non-volatile memory before the power drops off completely.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Most of the documentation on the Kinetis systems and the KL17 specifically refers to the NMI as being triggered from the system reset.&amp;nbsp; Is this the only way this interrupt will be triggered or can it be used while the processor is running?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 14:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-the-NMI-be-used-to-generate-an-interrupt-while-running/m-p/482902#M29529</guid>
      <dc:creator>jmaranhao1</dc:creator>
      <dc:date>2016-04-27T14:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can the NMI be used to generate an interrupt while running?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-the-NMI-be-used-to-generate-an-interrupt-while-running/m-p/482903#M29530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif'; font-size: 10pt;"&gt;Please be note that the NMI &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;interrupt&lt;/SPAN&gt; occurs when the pin is connected or forced to a low level input. The interrupt source can be either an interrupt or wake up source, not just the reset.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2016 07:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-the-NMI-be-used-to-generate-an-interrupt-while-running/m-p/482903#M29530</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-05-04T07:07:46Z</dc:date>
    </item>
  </channel>
</rss>