<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Possible KBI problems with GPIO changing between input and output? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Possible-KBI-problems-with-GPIO-changing-between-input-and/m-p/482894#M29527</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MKE04Z8VTG4 for capacitive sensing application using RC acquisition principle.&lt;/P&gt;&lt;P&gt;Sensing electrodes are connected on PTA2 and 3 and I am using KBI interrupt to measure the time.&lt;/P&gt;&lt;P&gt;I do not know how the KBI settings will be effected if I change the sensing pins to output (no changes to the KBI registers will be made)?&lt;/P&gt;&lt;P&gt;For example first I initialize KBI module and sensing pins as output. Then I start the sequence described in the pictures.&lt;/P&gt;&lt;P&gt;Basically I have no idea how the KBI works as this is the first time I am using it. And I do not know if there will be any problems with the KBI module (for example false interrupt execution) if I change the sensing pins to input/output or if I will have to reconfigure it when I change the sensing pins from input to output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6880i13D0856B3C890163/image-size/large?v=v2&amp;amp;px=999" title="capsense.jpg" alt="capsense.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jan 2016 00:33:56 GMT</pubDate>
    <dc:creator>jurestojs</dc:creator>
    <dc:date>2016-01-12T00:33:56Z</dc:date>
    <item>
      <title>Possible KBI problems with GPIO changing between input and output?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Possible-KBI-problems-with-GPIO-changing-between-input-and/m-p/482894#M29527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MKE04Z8VTG4 for capacitive sensing application using RC acquisition principle.&lt;/P&gt;&lt;P&gt;Sensing electrodes are connected on PTA2 and 3 and I am using KBI interrupt to measure the time.&lt;/P&gt;&lt;P&gt;I do not know how the KBI settings will be effected if I change the sensing pins to output (no changes to the KBI registers will be made)?&lt;/P&gt;&lt;P&gt;For example first I initialize KBI module and sensing pins as output. Then I start the sequence described in the pictures.&lt;/P&gt;&lt;P&gt;Basically I have no idea how the KBI works as this is the first time I am using it. And I do not know if there will be any problems with the KBI module (for example false interrupt execution) if I change the sensing pins to input/output or if I will have to reconfigure it when I change the sensing pins from input to output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6880i13D0856B3C890163/image-size/large?v=v2&amp;amp;px=999" title="capsense.jpg" alt="capsense.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 00:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Possible-KBI-problems-with-GPIO-changing-between-input-and/m-p/482894#M29527</guid>
      <dc:creator>jurestojs</dc:creator>
      <dc:date>2016-01-12T00:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Possible KBI problems with GPIO changing between input and output?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Possible-KBI-problems-with-GPIO-changing-between-input-and/m-p/482895#M29528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jure,&lt;/P&gt;&lt;P&gt;I think it can't work out.&lt;/P&gt;&lt;P&gt;If you have already set the PTA2 and PT3 as the KBI pin, it can't be GPIO pin simultaneously.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 07:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Possible-KBI-problems-with-GPIO-changing-between-input-and/m-p/482895#M29528</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-14T07:41:18Z</dc:date>
    </item>
  </channel>
</rss>