<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482493#M29508</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why do you need 32 bits SPI ? You can just send 4 bytes and manually control SS or CS pin with a dedicated gpio.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Apr 2016 20:47:01 GMT</pubDate>
    <dc:creator>mr_max</dc:creator>
    <dc:date>2016-04-27T20:47:01Z</dc:date>
    <item>
      <title>Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482491#M29506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking for a low cost USB controller with 32-bit SPI series ports.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 11:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482491#M29506</guid>
      <dc:creator>larryhe</dc:creator>
      <dc:date>2016-04-27T11:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482492#M29507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know you KL2 series has USB, but its SPI is 8 bits.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 12:41:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482492#M29507</guid>
      <dc:creator>larryhe</dc:creator>
      <dc:date>2016-04-27T12:41:38Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482493#M29508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why do you need 32 bits SPI ? You can just send 4 bytes and manually control SS or CS pin with a dedicated gpio.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 20:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482493#M29508</guid>
      <dc:creator>mr_max</dc:creator>
      <dc:date>2016-04-27T20:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482494#M29509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes this is a way, but your solution will need CPU involvement frequently.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some 16-bit ADC or DAC needs 24-bit CMD/data in one SPI CS period.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My assumption is: start the SPI then CPU go to deal other works. uC works efficiently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May you tell me your a few of your uC's which are capable of 32-bit SPI but low cost?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 01:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482494#M29509</guid>
      <dc:creator>larryhe</dc:creator>
      <dc:date>2016-04-28T01:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482495#M29510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi Larry!&lt;/P&gt;&lt;P&gt;If you dont want to interact with the processor you can use DMA.&lt;/P&gt;&lt;P&gt;Anyway max SPI speed is the BUS/2 and 1 trasnsaction(8 bit) is BUS/16 that will not demand a lot of CPU power. Even more you have an FIFO on both TX and RX so you can put your 24 bit data there and wait for tx-interrupt that will lead to BUS/48 in the interrupt mode.&lt;/P&gt;&lt;P&gt; MKL 26 is a good choice-low cost and it' USB is crystalless.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I hope it help,&lt;/P&gt;&lt;P&gt;Regards Alexey.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 17:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482495#M29510</guid>
      <dc:creator>alexeyusoltsev</dc:creator>
      <dc:date>2016-04-28T17:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482496#M29511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;So at present, the 32 bit SPI is a bottleneck. Please make reference from the thread below:&lt;A href="https://community.nxp.com/thread/327642"&gt;Transmit 32 Bit via SPI&lt;/A&gt; . Hope it is helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 09:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482496#M29511</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-05-03T09:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have a controller which has below features? USB, Cortex M0+, 32bit-SPI.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482497#M29512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I decide to select MK22FN512 to use its parallel bus (Flexbus). my question is fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 May 2016 11:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Do-you-have-a-controller-which-has-below-features-USB-Cortex-M0/m-p/482497#M29512</guid>
      <dc:creator>larryhe</dc:creator>
      <dc:date>2016-05-07T11:52:32Z</dc:date>
    </item>
  </channel>
</rss>