<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 cannot program dac of MK64FN1M0VLL12</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-dac-of-MK64FN1M0VLL12/m-p/480682#M29394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I have a problem with the dac of the mk64. first of all, I use a self designed board with the mk64 as the mcu. the mcu is clocked by a external crystal with 24MHz. I use an external voltage reference&amp;nbsp; I use jtag and the Segger j-link as the programmer. further, I also use the frdm64 evaluation board to test my programs. Of course, the on board sda is used to program the mk64. I use kinetis design studio, ksdk 1.2 and processor expert to write my codes. With the frdm64 all programs I ve written work just fine. however, when I tried to program the dac, it seemed to be unresponsive. no matter which digital value I set for the dac, the analog output stayed zero. there weren't any indications that the debugging process had gone wrong. So far I have tested the I2C and the ftm timer of mk64 on my board, and everything has gone smoothly. To make sure that you don't get wrong, I haven't used the same KDS project for the frdm64 board and my own. Only the settings for the DAC is identical.&lt;/P&gt;&lt;P&gt;Hope, someone has a solution for this problem&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;Hung&lt;/P&gt;&lt;P&gt;Here is the PE DAC configuration is attached. there isn't much codes that I need to write to start the DAC apart from this command:&amp;nbsp;&amp;nbsp; DAC_DRV_Output(FSL_DACONV1,2048);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 12 Dec 2015 11:04:43 GMT</pubDate>
    <dc:creator>hunglam</dc:creator>
    <dc:date>2015-12-12T11:04:43Z</dc:date>
    <item>
      <title>cannot program dac of MK64FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-dac-of-MK64FN1M0VLL12/m-p/480682#M29394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;I have a problem with the dac of the mk64. first of all, I use a self designed board with the mk64 as the mcu. the mcu is clocked by a external crystal with 24MHz. I use an external voltage reference&amp;nbsp; I use jtag and the Segger j-link as the programmer. further, I also use the frdm64 evaluation board to test my programs. Of course, the on board sda is used to program the mk64. I use kinetis design studio, ksdk 1.2 and processor expert to write my codes. With the frdm64 all programs I ve written work just fine. however, when I tried to program the dac, it seemed to be unresponsive. no matter which digital value I set for the dac, the analog output stayed zero. there weren't any indications that the debugging process had gone wrong. So far I have tested the I2C and the ftm timer of mk64 on my board, and everything has gone smoothly. To make sure that you don't get wrong, I haven't used the same KDS project for the frdm64 board and my own. Only the settings for the DAC is identical.&lt;/P&gt;&lt;P&gt;Hope, someone has a solution for this problem&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;Hung&lt;/P&gt;&lt;P&gt;Here is the PE DAC configuration is attached. there isn't much codes that I need to write to start the DAC apart from this command:&amp;nbsp;&amp;nbsp; DAC_DRV_Output(FSL_DACONV1,2048);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2015 11:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-dac-of-MK64FN1M0VLL12/m-p/480682#M29394</guid>
      <dc:creator>hunglam</dc:creator>
      <dc:date>2015-12-12T11:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: cannot program dac of MK64FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-dac-of-MK64FN1M0VLL12/m-p/480683#M29395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hung,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you selected the reference voltage for DAC? It has the option to select between two different sources. Please see this post for more reference: &lt;A href="https://community.nxp.com/message/565288"&gt;Re: TWR-K60F120M getting the DAC to work&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2015 20:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/cannot-program-dac-of-MK64FN1M0VLL12/m-p/480683#M29395</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2015-12-15T20:24:42Z</dc:date>
    </item>
  </channel>
</rss>