<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does KL03 need a pullup resistor on reset pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480230#M29375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ted,&lt;/P&gt;&lt;P&gt;If you are using SDK_1.3_FRDM-KL03Z download from &lt;A href="http://cache.nxp.com/files/32bit/software_tools/KINETIS-EXPERT-TOOL.html?fpsp=1&amp;amp;WT_TYPE=Software%20Development%20Kits&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=html&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.html"&gt;Kinetis SDK Builder (REV 2 &amp;amp; 1.3)&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;You can search "RESET Pin filter" in Kinetis SDK v.1.3 API Reference Manual.pdf. (for example ...\SDK_1.3_FRDM-KL03Z\doc)&lt;/P&gt;&lt;P&gt;The function RCM_HAL_SetResetPinFilterConfig() can be found in such folder. (for example&amp;nbsp; ...\SDK_1.3_FRDM-KL03Z\platform\hal\src\rcm)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54388i15444DAE9F2DC0AF/image-size/large?v=v2&amp;amp;px=999" title="RCM_HAL_SetResetPinFilterConfig.jpg" alt="RCM_HAL_SetResetPinFilterConfig.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 03:06:19 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2016-04-28T03:06:19Z</dc:date>
    <item>
      <title>Does KL03 need a pullup resistor on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480227#M29372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I designed a PCB that takes the MKL03Z32CAF4, I thought the reset pin had an internal pull up resistor but now I'm not sure.&amp;nbsp; Does it?&amp;nbsp; Is there a document that describes things such as this and the minimum requirements?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 19:49:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480227#M29372</guid>
      <dc:creator>tedmawson</dc:creator>
      <dc:date>2016-04-26T19:49:02Z</dc:date>
    </item>
    <item>
      <title>Re: Does KL03 need a pullup resistor on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480228#M29373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ted,&lt;/P&gt;&lt;P&gt;The RESET_b pin, if enabled, should have a 100 nF capacitor close to the MCU for transient protection. When enabled as it's default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended. &lt;/P&gt;&lt;P&gt;For more detail, please refer &lt;A href="http://cache.nxp.com/files/32bit/doc/quick_ref_guide/KLQRUG.pdf?fpsp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;Kinetis L Peripheral Module Quick Reference&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35633i39C4E4F23B6D46BF/image-size/large?v=v2&amp;amp;px=999" title="RESET_b and NMI_b.jpg" alt="RESET_b and NMI_b.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 02:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480228#M29373</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-04-27T02:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Does KL03 need a pullup resistor on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480229#M29374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the clarification.&amp;nbsp; I'm trying to make my hardware start up reliably so, given I'm using the KSDK (without PE), what is the recommended way to apply/configure the digital filter available in the RCM_RPFC register.&amp;nbsp; I'm hoping that doing this will allow my prototype PCBs to start up reliably but I will add the components suggested for the next spin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 13:17:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480229#M29374</guid>
      <dc:creator>tedmawson</dc:creator>
      <dc:date>2016-04-27T13:17:54Z</dc:date>
    </item>
    <item>
      <title>Re: Does KL03 need a pullup resistor on reset pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480230#M29375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ted,&lt;/P&gt;&lt;P&gt;If you are using SDK_1.3_FRDM-KL03Z download from &lt;A href="http://cache.nxp.com/files/32bit/software_tools/KINETIS-EXPERT-TOOL.html?fpsp=1&amp;amp;WT_TYPE=Software%20Development%20Kits&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=html&amp;amp;WT_ASSET=Downloads&amp;amp;fileExt=.html"&gt;Kinetis SDK Builder (REV 2 &amp;amp; 1.3)&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;You can search "RESET Pin filter" in Kinetis SDK v.1.3 API Reference Manual.pdf. (for example ...\SDK_1.3_FRDM-KL03Z\doc)&lt;/P&gt;&lt;P&gt;The function RCM_HAL_SetResetPinFilterConfig() can be found in such folder. (for example&amp;nbsp; ...\SDK_1.3_FRDM-KL03Z\platform\hal\src\rcm)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54388i15444DAE9F2DC0AF/image-size/large?v=v2&amp;amp;px=999" title="RCM_HAL_SetResetPinFilterConfig.jpg" alt="RCM_HAL_SetResetPinFilterConfig.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 03:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Does-KL03-need-a-pullup-resistor-on-reset-pin/m-p/480230#M29375</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-04-28T03:06:19Z</dc:date>
    </item>
  </channel>
</rss>