<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is AREF pin break-out usable on FRDM-K64F? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-AREF-pin-break-out-usable-on-FRDM-K64F/m-p/479966#M29354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, there has no register to setting for this purpose. (Besides the &lt;SPAN style="font-size: 10pt;"&gt;ADC_REFSEL). For other reference voltage other than VDD or 1.2V, you should route out the pin from J2. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2016 08:25:43 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2016-02-04T08:25:43Z</dc:date>
    <item>
      <title>Is AREF pin break-out usable on FRDM-K64F?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-AREF-pin-break-out-usable-on-FRDM-K64F/m-p/479965#M29353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I read the board schematic correctly, the VREFH pin is tied to VDD through a jumper resistor (R54), and the jumper resistor (R53) which ties VREFH to the AREF break-out pin on connector J2 is not populated. I need to be able to apply an external 2.048 reference voltage via the AREF pin, but the way I see it, this won't be possible without performing surgery on the board. :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also looked at the board reference guide and at the K64F sub-family datasheet, but was unable to find any way to achieve an internal reference voltage of 2.048V, except if I power the whole board from that voltage. It is either VDD or 1.2V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any chance I missed something and this is achievable either on the AREF pin-out without taking a soldering iron to the board, or through some register setting in the MCU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 18:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-AREF-pin-break-out-usable-on-FRDM-K64F/m-p/479965#M29353</guid>
      <dc:creator>TodorTodorov</dc:creator>
      <dc:date>2016-02-01T18:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: Is AREF pin break-out usable on FRDM-K64F?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-AREF-pin-break-out-usable-on-FRDM-K64F/m-p/479966#M29354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, there has no register to setting for this purpose. (Besides the &lt;SPAN style="font-size: 10pt;"&gt;ADC_REFSEL). For other reference voltage other than VDD or 1.2V, you should route out the pin from J2. &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 08:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-AREF-pin-break-out-usable-on-FRDM-K64F/m-p/479966#M29354</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-02-04T08:25:43Z</dc:date>
    </item>
  </channel>
</rss>