<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Enabling pull resistors in KDS 3.2.0</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enabling-pull-resistors-in-KDS-3-2-0/m-p/479880#M29346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill Sousan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using our community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please always mention the device you are using, so we can provide accurate answers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are talking about the KE02 as in your other &lt;A _jive_internal="true" href="https://community.nxp.com/thread/391753"&gt;&lt;STRONG&gt;post&lt;/STRONG&gt; &lt;/A&gt;​then this device only has internal pull-ups, not pull-downs, so that is why you cannot choose a direction in the &lt;STRONG&gt;Init_GPIO&lt;/STRONG&gt; component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About pin names, the KE02 has a pair of 32-bit registers called &lt;STRONG&gt;GPIOA&lt;/STRONG&gt; and &lt;STRONG&gt;GPIOB&lt;/STRONG&gt; wrapping 8-bit port pins. See below from the reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59093i9E40378F8CB43692/image-size/large?v=v2&amp;amp;px=999" title="KE02_GPIO.png" alt="KE02_GPIO.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 May 2016 16:24:28 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-05-17T16:24:28Z</dc:date>
    <item>
      <title>Enabling pull resistors in KDS 3.2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enabling-pull-resistors-in-KDS-3-2-0/m-p/479879#M29345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't find where one can identify the pull direction (pull-up or poll-down) within the KDS.&amp;nbsp; I need to add some pull-up resistors to a few GPIO inputs.&amp;nbsp; I see where I can add component Init_GPIO and in there identify which pin to initialize with a pull resistor but can't&amp;nbsp; find which direction (up or down).&amp;nbsp; Also its a bit confusing that the pin numbers are not the same as the chip pin numbers so I had to click on a few to figure out the mapping (this is a bit clunky if this is the normal operation)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 15:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enabling-pull-resistors-in-KDS-3-2-0/m-p/479879#M29345</guid>
      <dc:creator>blsousan</dc:creator>
      <dc:date>2016-05-17T15:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling pull resistors in KDS 3.2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enabling-pull-resistors-in-KDS-3-2-0/m-p/479880#M29346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill Sousan:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using our community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please always mention the device you are using, so we can provide accurate answers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are talking about the KE02 as in your other &lt;A _jive_internal="true" href="https://community.nxp.com/thread/391753"&gt;&lt;STRONG&gt;post&lt;/STRONG&gt; &lt;/A&gt;​then this device only has internal pull-ups, not pull-downs, so that is why you cannot choose a direction in the &lt;STRONG&gt;Init_GPIO&lt;/STRONG&gt; component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About pin names, the KE02 has a pair of 32-bit registers called &lt;STRONG&gt;GPIOA&lt;/STRONG&gt; and &lt;STRONG&gt;GPIOB&lt;/STRONG&gt; wrapping 8-bit port pins. See below from the reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59093i9E40378F8CB43692/image-size/large?v=v2&amp;amp;px=999" title="KE02_GPIO.png" alt="KE02_GPIO.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 16:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Enabling-pull-resistors-in-KDS-3-2-0/m-p/479880#M29346</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-05-17T16:24:28Z</dc:date>
    </item>
  </channel>
</rss>