<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: CAN example for mk22fx512vlh12</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478953#M29286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, that was how I downloaded but the website was automatically selecting MK22FX512Axxx12, but now I was able to download the MK22FX512xxx12 file. Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Nakul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 09:52:16 GMT</pubDate>
    <dc:creator>nakulyadur</dc:creator>
    <dc:date>2016-04-05T09:52:16Z</dc:date>
    <item>
      <title>CAN example for mk22fx512vlh12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478949#M29282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to Kinetis and trying to learn to program Kinetis microcontroller. I have installed KDS and updated KSDK as per instructions. But there are no examples or demos for mk22fx512vlh12 microcontroller available.&lt;/P&gt;&lt;P&gt;Can anyone provide me with an example program for mk22fx512vlh12 (CAN example would be very helpful)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 15:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478949#M29282</guid>
      <dc:creator>nakulyadur</dc:creator>
      <dc:date>2016-04-04T15:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: CAN example for mk22fx512vlh12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478950#M29283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nakul,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; About the sample code for MK22FX512VLH12, you can refer to the KSDK tower-K21f120m sample code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Could you tell me which KSDK version you are using now?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can download the KSDK2.0, and select the MK22FX512xxx12 in build an KSDK, you will get the SDK_2.0_MK22FX512xxx12, ksdk2.0 link is :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://kex.freescale.com/en/welcome"&gt; http://kex.freescale.com/en/welcome&lt;/A&gt;​&lt;/P&gt;&lt;P&gt;&amp;nbsp; After you download the KSDK2.0,&amp;nbsp; you can find the flexcan in folder:SDK_2.0_MK22FX512xxx12\boards\twrk21f120m\driver_examples\flexcan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 06:52:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478950#M29283</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-04-05T06:52:39Z</dc:date>
    </item>
    <item>
      <title>Re: CAN example for mk22fx512vlh12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478951#M29284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I am using KSDK version 1.3 and I have also downloaded KSDK 2.0 but I didn't know how to set it in the KDS as I couldn't find the file eclipse_update inside the tools folder. Please let me know how do I set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PE Multilink Universal for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And, when I select MK22FX512xxx12 and download the file, the downloaded file is named as MK22FX512Axxx12, is there a difference between them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nakul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 08:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478951#M29284</guid>
      <dc:creator>nakulyadur</dc:creator>
      <dc:date>2016-04-05T08:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: CAN example for mk22fx512vlh12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478952#M29285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nakul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you download interface like this in the KSDK2.0?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27899iEA01307E3676EB02/image-size/large?v=v2&amp;amp;px=999" title="46.jpg" alt="46.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you are using the KSDK2.0, you don't need to add the eclipse_updated in the KDS, just open the KSDK2.0 kds project directly!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MK22FX512Axxx12 have a little difference to the MK22FX512xxx12, for details, you can compare the head file, there has some register difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 09:16:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478952#M29285</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-04-05T09:16:26Z</dc:date>
    </item>
    <item>
      <title>Re: CAN example for mk22fx512vlh12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478953#M29286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, that was how I downloaded but the website was automatically selecting MK22FX512Axxx12, but now I was able to download the MK22FX512xxx12 file. Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Nakul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 09:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-example-for-mk22fx512vlh12/m-p/478953#M29286</guid>
      <dc:creator>nakulyadur</dc:creator>
      <dc:date>2016-04-05T09:52:16Z</dc:date>
    </item>
  </channel>
</rss>