<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 TWR-K60D100M Ethernet Connection Problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-Ethernet-Connection-Problem/m-p/478541#M29220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would be very grateful of some advice with the following problem.&lt;/P&gt;&lt;P&gt;I cannot establish a connection between the TWR-K60D100M and my local network using the TWR-SER board Ethernet interface.&lt;/P&gt;&lt;P&gt;I have tried both the ‘eth_to_serial’ and ‘httpsrv’ MQX RTCS examples, plus I have created a new MQX project using the wizard selecting the ‘Add RTCS Support’, ‘Basic Application’, IP type set to ‘DHCP’. The latter of these projects outputs the following info:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Waiting for ethernet cable plug in ... Cable connected&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Contacting DHCP server ...&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;RTCS failed to bind interface with IPv4, error = 1D04&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The defines in the main.h are:&lt;/P&gt;&lt;P&gt;#define ENET_IPADDR IPADDR(192,168,1,200)&lt;/P&gt;&lt;P&gt;#define ENET_IPMASK IPADDR(255,255,255,0)&lt;/P&gt;&lt;P&gt;#define ENET_GATEWAY IPADDR(192,168,1,1)&amp;nbsp; tried also 192,168,0,1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also tried a number of IP addresses which are within the router’s range of IP addresses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem seems to be that the TWR-K60D100M is not being issued with an IP address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The hardware jumpers are set as followers (as per the tower documentation):&lt;/P&gt;&lt;P&gt;TWR-K60D100M&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J10 Pins 2-3&lt;/P&gt;&lt;P&gt;TWR-SER&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J2 Pins 3-4 (CLK_SEL)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J3 Pins 2-3 (CLKIN_SEL)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J12 Pins 9-10 (ETH_CONFIG)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the boards are mounted correctly to the elevator boards (primary/secondary).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software versions are:&lt;/P&gt;&lt;P&gt;CodeWarrior 10.6.4.&lt;/P&gt;&lt;P&gt;MQX 4.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built the twrk60d100m bsp, psp, rtcs and shell libraries which are stored at:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\lib\twrk60d100m.cw10gcc\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can run the simple ‘Hello’ example no problem.&lt;/P&gt;&lt;P&gt;I also have a Freescale license so no problem with compiler limitations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Mike.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 31 Jan 2016 15:43:04 GMT</pubDate>
    <dc:creator>mikekay</dc:creator>
    <dc:date>2016-01-31T15:43:04Z</dc:date>
    <item>
      <title>TWR-K60D100M Ethernet Connection Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-Ethernet-Connection-Problem/m-p/478541#M29220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would be very grateful of some advice with the following problem.&lt;/P&gt;&lt;P&gt;I cannot establish a connection between the TWR-K60D100M and my local network using the TWR-SER board Ethernet interface.&lt;/P&gt;&lt;P&gt;I have tried both the ‘eth_to_serial’ and ‘httpsrv’ MQX RTCS examples, plus I have created a new MQX project using the wizard selecting the ‘Add RTCS Support’, ‘Basic Application’, IP type set to ‘DHCP’. The latter of these projects outputs the following info:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Waiting for ethernet cable plug in ... Cable connected&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Contacting DHCP server ...&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;RTCS failed to bind interface with IPv4, error = 1D04&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The defines in the main.h are:&lt;/P&gt;&lt;P&gt;#define ENET_IPADDR IPADDR(192,168,1,200)&lt;/P&gt;&lt;P&gt;#define ENET_IPMASK IPADDR(255,255,255,0)&lt;/P&gt;&lt;P&gt;#define ENET_GATEWAY IPADDR(192,168,1,1)&amp;nbsp; tried also 192,168,0,1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also tried a number of IP addresses which are within the router’s range of IP addresses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem seems to be that the TWR-K60D100M is not being issued with an IP address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The hardware jumpers are set as followers (as per the tower documentation):&lt;/P&gt;&lt;P&gt;TWR-K60D100M&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J10 Pins 2-3&lt;/P&gt;&lt;P&gt;TWR-SER&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J2 Pins 3-4 (CLK_SEL)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J3 Pins 2-3 (CLKIN_SEL)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J12 Pins 9-10 (ETH_CONFIG)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the boards are mounted correctly to the elevator boards (primary/secondary).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software versions are:&lt;/P&gt;&lt;P&gt;CodeWarrior 10.6.4.&lt;/P&gt;&lt;P&gt;MQX 4.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have built the twrk60d100m bsp, psp, rtcs and shell libraries which are stored at:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\lib\twrk60d100m.cw10gcc\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can run the simple ‘Hello’ example no problem.&lt;/P&gt;&lt;P&gt;I also have a Freescale license so no problem with compiler limitations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Mike.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 31 Jan 2016 15:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-Ethernet-Connection-Problem/m-p/478541#M29220</guid>
      <dc:creator>mikekay</dc:creator>
      <dc:date>2016-01-31T15:43:04Z</dc:date>
    </item>
  </channel>
</rss>