<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB_device (CDC) project for Kinetis K40 tower board</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153025#M291</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should better to use MQX if RTOS is needed, otherwise use USB Bare metal stack at &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't use the Kinetis_sc code, it is for validation purpose only. It is not well written.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Aug 2011 16:31:30 GMT</pubDate>
    <dc:creator>Dekiru</dc:creator>
    <dc:date>2011-08-29T16:31:30Z</dc:date>
    <item>
      <title>USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153020#M286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There is an USB_device project example for K40 development kit, which is included in the KINETIS512_SC folder&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anybody tried and used the&amp;nbsp;the example&amp;nbsp;successfully?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;can't get it to work since the enumeration process doesn't get finished and eventually issues&amp;nbsp;the message "USB Device Not Recognized"&lt;/P&gt;&lt;P&gt;Thank you for any help you can provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2011 00:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153020#M286</guid>
      <dc:creator>ttu</dc:creator>
      <dc:date>2011-07-23T00:21:37Z</dc:date>
    </item>
    <item>
      <title>Re: USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153021#M287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have had the same problem with no resolution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The NXP parts are much easier to get working!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2011 21:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153021#M287</guid>
      <dc:creator>emh203</dc:creator>
      <dc:date>2011-07-27T21:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153022#M288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure you point it to the driver located in the project directory: &lt;STRONG&gt;\kinetis-sc\src\projects\USB_device﻿&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also look at the readme.txt to make sure the TWR-SER is setup properly. I was able to confirm it working on my TWR-K40&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-amh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 00:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153022#M288</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2011-07-28T00:43:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153023#M289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am personally having trouble in this realm under MQX and going thru Hubs -- it doesn't appear that MQX cycles thru all the ports, just the first 'active'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, note that&amp;nbsp;the CDC examples ONLY work with 'standard' protocol-type devices (2) -- anything that returns 'vendor specific' will be ignored.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2011 00:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153023#M289</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2011-08-23T00:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153024#M290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you would like to try, we have an USB CDC working demo for KwikStik kit, which is a K40 development kit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The link to download is:&lt;/P&gt;&lt;P&gt;&lt;A href="http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20%2B%20Wave.rar" rel="nofollow" target="_blank"&gt;http://brtos.googlecode.com/files/BRTOS%201.6x%20K40%20-%20SD%20%2B%20Wave.rar&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This demo has SD card access with FAT16/32 file system and a terminal trough USB CDC class.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2011 20:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153024#M290</guid>
      <dc:creator>gustavod</dc:creator>
      <dc:date>2011-08-25T20:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: USB_device (CDC) project for Kinetis K40 tower board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153025#M291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should better to use MQX if RTOS is needed, otherwise use USB Bare metal stack at &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't use the Kinetis_sc code, it is for validation purpose only. It is not well written.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2011 16:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-device-CDC-project-for-Kinetis-K40-tower-board/m-p/153025#M291</guid>
      <dc:creator>Dekiru</dc:creator>
      <dc:date>2011-08-29T16:31:30Z</dc:date>
    </item>
  </channel>
</rss>