<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックAre 32-bit SPI slave frames possible on MK60DN512VMD10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476983#M29076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I have 3 questions concerning the reference manual for the Kinetis MK60DN512VMD10 used in the TWR-K60D100M &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;Document Number: K60P144M100SF2V2RM Rev. 2 Jun 2012&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; K60 Sub-Family Reference Manual, Rev. 2 Jun 2012 -&amp;nbsp; Preliminary General Business Information&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I'm trying to connect a 24-bit SigmaDelta ADC converter PCM1804 (master) to SPI (slave) on Tower_TWR-K60D100M.&lt;/P&gt;&lt;P&gt;It sends a 32-bit frames and so it is incompatible with KSDK_1.3.0 driver in&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; ...\Freescale\KSDK_1.3.0\examples\twrk60d100m\driver_examples\dspi\...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;which accepts only 16-bit frames.&lt;/P&gt;&lt;P&gt;So I've started to program the SPI "manually" and I found out that there are problems!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The manual &lt;EM&gt;K60P144M100SF2V2RM Rev.2&lt;/EM&gt;&amp;nbsp; says explicitly, that 32bit frames are supported in the in slave mode.:&lt;/P&gt;&lt;P&gt;Figure 50-1, page 1402 - shows 32-bit path from Shift Register&amp;nbsp; to RX FIFO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.3.4, page 1418 - shows SPIx_CTARn_SLAVE where FMSZ has 5 bits == 32bits frame size&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.3.9, page 1427 - says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;POPR is used to read the RX FIFO. Eight- or sixteen-bit read accesses to the POPR have&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the same effect on the RX FIFO as 32-bit read accesses.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.4.2, page 1431 - says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the SPI frames can be 32 bits long&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My test program gives only max. 16 bit frames which I can read.&lt;/P&gt;&lt;P&gt;The highest bit of FMSZ (bit 31) has no influence on the received data in the RXFIFO and POPR.&lt;/P&gt;&lt;P&gt;I see in the RXFIFO the high-word and low-word of a 32-bit frame (and I could assemble the 32-bit frame), but the Reference Manual says I should get 32-bit result in POPR.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So what is true ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 2:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The manual &lt;EM&gt;K60P144M100SF2V2RM Rev. 2&lt;/EM&gt;&amp;nbsp; shows (§50.3.1, page 1410)&amp;nbsp; the SPIx_MCR layout:&lt;/P&gt;&lt;P&gt; - bit 25 is ROOE and bits 24,23,22 are reserved&lt;/P&gt;&lt;P&gt;in the old manual, there was&lt;/P&gt;&lt;P&gt; - bit 25 was PCSSE and ROOE was on bit 24, bits 23,22 were reserved&lt;/P&gt;&lt;P&gt;Kinetis Desing Studio 3.1.0 shows in EmbSys Registers the "old" layout (MK60D10 chip selected)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So what is true ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 3:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have downloaded 2 versions of &lt;EM&gt;K60P144M100SF2V2RM Rev.2&lt;/EM&gt;,&lt;/P&gt;&lt;P&gt;one is 14.229KB big - another only 13.853KB !&lt;/P&gt;&lt;P&gt;(they seem to be the same... but who knows - I'm not going to compare page by page...)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So how can it be ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;A version is A VERSION and should have always the same size (at least in my opinion) !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for a quick responce.&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Piotr Fyda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Mar 2016 16:17:45 GMT</pubDate>
    <dc:creator>piotrfyda</dc:creator>
    <dc:date>2016-03-15T16:17:45Z</dc:date>
    <item>
      <title>Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476983#M29076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I have 3 questions concerning the reference manual for the Kinetis MK60DN512VMD10 used in the TWR-K60D100M &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;Document Number: K60P144M100SF2V2RM Rev. 2 Jun 2012&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; K60 Sub-Family Reference Manual, Rev. 2 Jun 2012 -&amp;nbsp; Preliminary General Business Information&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I'm trying to connect a 24-bit SigmaDelta ADC converter PCM1804 (master) to SPI (slave) on Tower_TWR-K60D100M.&lt;/P&gt;&lt;P&gt;It sends a 32-bit frames and so it is incompatible with KSDK_1.3.0 driver in&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; ...\Freescale\KSDK_1.3.0\examples\twrk60d100m\driver_examples\dspi\...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;which accepts only 16-bit frames.&lt;/P&gt;&lt;P&gt;So I've started to program the SPI "manually" and I found out that there are problems!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The manual &lt;EM&gt;K60P144M100SF2V2RM Rev.2&lt;/EM&gt;&amp;nbsp; says explicitly, that 32bit frames are supported in the in slave mode.:&lt;/P&gt;&lt;P&gt;Figure 50-1, page 1402 - shows 32-bit path from Shift Register&amp;nbsp; to RX FIFO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.3.4, page 1418 - shows SPIx_CTARn_SLAVE where FMSZ has 5 bits == 32bits frame size&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.3.9, page 1427 - says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;POPR is used to read the RX FIFO. Eight- or sixteen-bit read accesses to the POPR have&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the same effect on the RX FIFO as 32-bit read accesses.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;§50.4.2, page 1431 - says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;the SPI frames can be 32 bits long&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My test program gives only max. 16 bit frames which I can read.&lt;/P&gt;&lt;P&gt;The highest bit of FMSZ (bit 31) has no influence on the received data in the RXFIFO and POPR.&lt;/P&gt;&lt;P&gt;I see in the RXFIFO the high-word and low-word of a 32-bit frame (and I could assemble the 32-bit frame), but the Reference Manual says I should get 32-bit result in POPR.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So what is true ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 2:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The manual &lt;EM&gt;K60P144M100SF2V2RM Rev. 2&lt;/EM&gt;&amp;nbsp; shows (§50.3.1, page 1410)&amp;nbsp; the SPIx_MCR layout:&lt;/P&gt;&lt;P&gt; - bit 25 is ROOE and bits 24,23,22 are reserved&lt;/P&gt;&lt;P&gt;in the old manual, there was&lt;/P&gt;&lt;P&gt; - bit 25 was PCSSE and ROOE was on bit 24, bits 23,22 were reserved&lt;/P&gt;&lt;P&gt;Kinetis Desing Studio 3.1.0 shows in EmbSys Registers the "old" layout (MK60D10 chip selected)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So what is true ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 3:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have downloaded 2 versions of &lt;EM&gt;K60P144M100SF2V2RM Rev.2&lt;/EM&gt;,&lt;/P&gt;&lt;P&gt;one is 14.229KB big - another only 13.853KB !&lt;/P&gt;&lt;P&gt;(they seem to be the same... but who knows - I'm not going to compare page by page...)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So how can it be ???&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;A version is A VERSION and should have always the same size (at least in my opinion) !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for a quick responce.&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Piotr Fyda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 16:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476983#M29076</guid>
      <dc:creator>piotrfyda</dc:creator>
      <dc:date>2016-03-15T16:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476984#M29077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Piotr Fyda:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your K60 questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1)&lt;/STRONG&gt; It must be possible to receive 32-bit SPI frames. Be careful not to have an open view of the &lt;STRONG&gt;SPIx_POPR&lt;/STRONG&gt; register in the debugger, otherwise the corresponding data in the &lt;STRONG&gt;RX FIFO&lt;/STRONG&gt; might be lost and the part of your code which reads the received values will fail.&lt;/P&gt;&lt;P&gt;If it still fails please share your code or project to give it a check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2)&lt;/STRONG&gt; I think you are right about this. I will report it to our developers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3)&lt;/STRONG&gt; Could you please point me to the site where you got the manuals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our official NXP website I can only see one file for &lt;STRONG&gt;K60P144M100SF2&lt;SPAN style="color: #e23d39;"&gt;V2&lt;/SPAN&gt;RM.pdf&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/k-series/k6x-ethernet-mcus/kinetis-k60-100-mhz-ethernet-usb-analog-integration-mcus:K60_100?fpsp=1&amp;amp;tab=Documentation_Tab" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/k-series/k6x-ethernet-mcus/kinetis-k60-100-mhz-ethernet-usb-analog-integration-mcus:K60_100?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;K60_100 |Kinetis K60 100 MHz MCUs|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe you also downloaded the Reference Manual &lt;STRONG&gt;K60P144M100SF2RM.pdf&lt;/STRONG&gt;. This is for an old revision of the K60_100 MHz silicon.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 23:29:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476984#M29077</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-30T23:29:09Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476985#M29078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First - thank you for your response and informing the developers about Point 2!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning my remaining points 1) and 3):&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Ad 1)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;You write:&amp;nbsp; &lt;EM&gt;Be careful not to have an open view of the &lt;STRONG&gt;SPIx_POPR&lt;/STRONG&gt; register in the debugger, otherwise the corresponding data in the &lt;STRONG&gt;RX FIFO&lt;/STRONG&gt; might be lost...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;It is for the first time I meet such a warning !&lt;/P&gt;&lt;P&gt;I assumed that debugger can be used to see what's going on in the system and it does not have impact on behaviour of the hardware (except for the real time performance of course).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You write also: &lt;EM&gt;It must be possible to receive 32-bit SPI Frames.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;It is not - 32-bit Frames do not work on MK60DN512VMD10 - you get 2 16-bit Frames and the&amp;nbsp; highest bit of FMSZ (bit 31) has no influence on the received data in the RXFIFO and POPR.&lt;/P&gt;&lt;P&gt;Here is my test program mainc.c:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "board.h"&lt;BR /&gt;#include "pin_mux.h"&lt;BR /&gt;#include "fsl_device_registers.h"&lt;BR /&gt;#include "fsl_clock_manager.h"&lt;BR /&gt;#include "fsl_interrupt_manager.h"&lt;BR /&gt;#include "fsl_debug_console.h"&lt;BR /&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;/* define SPI1 registers */&lt;BR /&gt;#define SPI1MRC&amp;nbsp; 0x4002D000&lt;BR /&gt;#define SPI1CTAR0&amp;nbsp; 0x4002D00C&lt;BR /&gt;#define SPI1SR&amp;nbsp;&amp;nbsp; 0x4002D02C&lt;BR /&gt;#define SPI1RSER&amp;nbsp; 0x4002D030&lt;BR /&gt;#define SPI1POPR&amp;nbsp; 0x4002D038&lt;BR /&gt;/* define some bits in SPIx registers */&lt;BR /&gt;#define HALT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000001&lt;BR /&gt;#define RXFIFO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00001000&lt;BR /&gt;#define CLR_TXF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000800&lt;BR /&gt;#define CLR_RXF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000400&lt;BR /&gt;#define RFDF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00020000&lt;BR /&gt;/* and some other needed defines */&lt;BR /&gt;#define GPIOAT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x400ff00c&lt;BR /&gt;#define PTA11&amp;nbsp; (1&amp;lt;&amp;lt;11)&lt;BR /&gt;#define RXBUFSIZE 64&lt;BR /&gt;#define UIP unsigned int *&lt;/P&gt;&lt;P&gt;unsigned int *rxptr, rxcnt, rxval, rxbuf[RXBUFSIZE+2];&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;int i;&lt;BR /&gt;rxcnt = rxval = 0;&lt;BR /&gt;rxptr = rxbuf;&lt;BR /&gt;for (i=0; i++; i&amp;lt;RXBUFSIZE) rxbuf[i] = 0;&lt;/P&gt;&lt;P&gt;CLOCK_SYS_EnablePortClock(PORTA_IDX);&lt;BR /&gt;CLOCK_SYS_EnablePortClock(PORTB_IDX);&lt;BR /&gt;CLOCK_SYS_EnablePortClock(PORTC_IDX);&lt;BR /&gt;CLOCK_SYS_EnablePortClock(PORTD_IDX);&lt;BR /&gt;CLOCK_SYS_EnablePortClock(PORTE_IDX);&lt;/P&gt;&lt;P&gt;BOARD_ClockInit();&lt;BR /&gt;dbg_uart_init();&lt;BR /&gt;GPIO_DRV_Init(switchPins, ledPins);&lt;/P&gt;&lt;P&gt;configure_spi_pins(1);&lt;BR /&gt;CLOCK_SYS_EnableSpiClock(1);&lt;/P&gt;&lt;P&gt;*(UIP)SPI1MRC =&amp;nbsp; HALT;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // halt SP1 for any case&lt;BR /&gt;*(UIP)SPI1MRC |= RXFIFO|CLR_TXF|CLR_RXF;&lt;BR /&gt;*(UIP)SPI1SR =&amp;nbsp; 0xFFFFFFFF;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clr all bits&lt;BR /&gt;*(UIP)SPI1RSER = RFDF ;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // generate interrupt from RFDF&lt;BR /&gt;*(UIP)&lt;STRONG&gt;SPI1CTAR0 = 0xF8000000;&amp;nbsp;&amp;nbsp; // frame32, inact.low, lead.edge&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*(UIP)SPI1MRC = (*(UIP)SPI1MRC) &amp;amp; ~HALT; // start SPI1&lt;BR /&gt;INT_SYS_EnableIRQ(27);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // SPI1 vector = 43 = 16+27&lt;BR /&gt;INT_SYS_EnableIRQGlobal();&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;printf("\nTest SPI1 slave / PCM1804 master\r\n");&lt;/P&gt;&lt;P&gt;while(1) {&lt;BR /&gt;GPIO_SW_DELAY;&lt;BR /&gt;printf("\nrxcnt %08x&amp;nbsp;&amp;nbsp; rxval %08x \r\n",rxcnt, rxval);&lt;BR /&gt;}&lt;BR /&gt;return 0;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void SPI1_IRQHandler(void) {&lt;BR /&gt;&lt;STRONG&gt;*(UIP)GPIOAT = PTA11;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // toggle test port (TGL on scope)&lt;/STRONG&gt;&lt;BR /&gt;rxval= *(UIP)SPI1POPR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // get received 32bit word&lt;BR /&gt;(*(UIP)SPI1SR) |= RFDF;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clr RFDF&lt;BR /&gt;rxcnt++;&lt;BR /&gt;*(rxptr++)= rxval;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // store in rxbuf&lt;BR /&gt;if (rxptr-rxbuf&amp;gt;RXBUFSIZE) rxptr= rxbuf; // circular buffer&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/*EOF*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you see, SPI1CTAR0 = 0xF8000000 - so frame= 32-bit, inact.low, lead.edge&lt;/P&gt;&lt;P&gt;but despite this setting I get two 16 bit frames (signal TGL below is toggled on each SPI1 Interrupt)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="m11s.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27709iABBD45F136D94821/image-size/large?v=v2&amp;amp;px=999" role="button" title="m11s.jpg" alt="m11s.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Scope screen shot shows a data frame starting with 0xfb.... - in the rxbuf we see high words with 0xfb... and low words with low byte equal to zero as the PCM1804 sends only 24 conversion bits and 8 zeros: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="rxbuf.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27766i9D8E2CA6C838BE27/image-size/large?v=v2&amp;amp;px=999" role="button" title="rxbuf.JPG" alt="rxbuf.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Ad 3)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Of course I've downloaded &lt;STRONG&gt;K60P144M100SF2RM.pdf&lt;/STRONG&gt; also - in other case I couldn't report the&amp;nbsp; problem in point 2 !&lt;/P&gt;&lt;P&gt;All downloads were done from the NXP page.&lt;/P&gt;&lt;P&gt;But the best comes now - I've just downloaded &lt;STRONG&gt;K60P144M100SF2&lt;SPAN style="color: #e23d39;"&gt;V2&lt;/SPAN&gt;RM.pdf&lt;/STRONG&gt; from NXP - link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/K60P144M100SF2V2RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;&lt;/A&gt;&lt;A href="http://cache.nxp.com/files/32bit/doc/ref_manual/K60P144M100SF2V2RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference" target="test_blank"&gt;http://cache.nxp.com/files/32bit/doc/ref_manual/K60P144M100SF2V2RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference&lt;/A&gt; Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This time it is &lt;STRONG&gt;20.5MB&lt;/STRONG&gt; big !! - despite that you see:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="k1.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26625i79FC98EBB8825DEA/image-size/large?v=v2&amp;amp;px=999" role="button" title="k1.JPG" alt="k1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So I have now 3 Versions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14.229KB - downloaded 2014-03-05&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 13.853KB - downloaded 2016-02-10&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20.502KB - downloaded 2016-03-31&lt;/P&gt;&lt;P&gt;When you open these files in an editor, you see that the content is different - one can only hope that the pdf view / printout will be the same - but nobody can check it page by page...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Piotr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS 1&lt;/P&gt;&lt;P&gt;The above experience and other points e.g. mentioned in&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/388145"&gt;Comments on TWR-K60D100, K60 and KSDK-1.3.0 documentation&lt;/A&gt; &lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/385338"&gt;Kinetis SDK v.1.3 API Reference Manual Rev.0 - the worst documentation I've ever seen !!!&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;are not the best publicity for Kinetis ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS 2&lt;/P&gt;&lt;P&gt;a) why it is not posssible to attach a file to a posting (e.g. my main.c) ??&lt;/P&gt;&lt;P&gt;b) why the automatical correction in the Editor here changes very often the first letterts to capitals ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 11:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476985#M29078</guid>
      <dc:creator>piotrfyda</dc:creator>
      <dc:date>2016-04-04T11:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476986#M29079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does it make a difference to properly load PUSHR prior to each data reception?&amp;nbsp; I also notice you disable the RXFIFO, but NOT the TXFIFO -- seems odd.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 12:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476986#M29079</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-04-05T12:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476987#M29080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Why should I load PUSHR when I do only receive as slave ???&lt;/P&gt;&lt;P&gt;Same concerning TXFIFO !  (transmitter is disabled)&lt;/P&gt;&lt;P&gt;There is no danger I get an overrun (no load in the test program at all) - so RXFIFO is disabled for easier handling.&lt;/P&gt;&lt;P&gt;But the same problem is  with RXFIFO enabled !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kind regards&lt;/P&gt;&lt;P&gt;Piotr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 13:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476987#M29080</guid>
      <dc:creator>piotrfyda</dc:creator>
      <dc:date>2016-04-05T13:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476988#M29081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SPI is INHERENTLY bidirectional, and SOMETHING &lt;SPAN style="text-decoration: underline;"&gt;will&lt;/SPAN&gt; TX for each RX.&amp;nbsp; I don't KNOW if giving PUSHR something 'valid' will affect receive data grouping, or even how the hardware handles a '32 bit length' callout from the 16-bit PUSHR -- but it seems worth testing.&amp;nbsp; Try pushing two words before each RX.&amp;nbsp; It is interesting to note that the K64 manual talks about PUSHR being full 32bits in 'slave' mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You mention a 'V2' reference manual -- are you running V2 chips? (No 'Z' in the P/N)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried running with CONT_SCKE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What happens if you run a 24-bit length?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 14:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476988#M29081</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-04-05T14:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: Are 32-bit SPI slave frames possible on MK60DN512VMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476989#M29082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You write:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't KNOW if giving PUSHR something 'valid' will affect receive data grouping, or even how the hardware handles a '32 bit length' callout from the 16-bit PUSHR -- but it seems worth testing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean I should test it ???     NXP sells the stuff, so it should know how it works !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The answer to your question " What happens if you run a 24-bit length?" is clear - I've told already:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"the  highest bit of FMSZ (bit 31 of SPI1CTAR0) has no influence on the received data in the RXFIFO and POPR"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and I receive for each /CS and 32 clocks two frames with 8 bits only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the e-mail I've received there are no lines:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You mention a 'V2' reference manual -- are you running V2 chips? (No 'Z' in the P/N)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried running with CONT_SCKE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which are visible on the   &lt;A href="https://community.freescale.com/message/" target="test_blank"&gt;https://community.freescale.com/message/&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here the answers:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;                Yes, I run V2 chip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;                Yes, no change - for me this bit seems to be only for master mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Piotr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 12:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-32-bit-SPI-slave-frames-possible-on-MK60DN512VMD10/m-p/476989#M29082</guid>
      <dc:creator>piotrfyda</dc:creator>
      <dc:date>2016-04-06T12:11:09Z</dc:date>
    </item>
  </channel>
</rss>