<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 ke02z run only in debug</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476354#M29003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using processor expert with keil. The problem is that my program runs in debug only. It's not running at por. As I read in the other threads, there is no "librarian" settings found in PE. I am running from internal oscillator. 32khz oscillator is connected but not configured to use. Another problem is that I have to flash the program before debugging(= flashing two times, one when starting debugging and another before that).&lt;/P&gt;&lt;P&gt;Using my own board, opensda that comes with fdrm-ke02z. Fdrm processor is disconnected removing jumper resistor&lt;/P&gt;&lt;P&gt;. Kindly help. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 13:11:42 GMT</pubDate>
    <dc:creator>surajka</dc:creator>
    <dc:date>2016-04-26T13:11:42Z</dc:date>
    <item>
      <title>ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476354#M29003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using processor expert with keil. The problem is that my program runs in debug only. It's not running at por. As I read in the other threads, there is no "librarian" settings found in PE. I am running from internal oscillator. 32khz oscillator is connected but not configured to use. Another problem is that I have to flash the program before debugging(= flashing two times, one when starting debugging and another before that).&lt;/P&gt;&lt;P&gt;Using my own board, opensda that comes with fdrm-ke02z. Fdrm processor is disconnected removing jumper resistor&lt;/P&gt;&lt;P&gt;. Kindly help. Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 13:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476354#M29003</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-26T13:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476355#M29004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suraj,&lt;/P&gt;&lt;P&gt;Before answer your question, I'd like to get the more information about the question.&lt;/P&gt;&lt;P&gt;Did the FRDM-KEXX Driver Library package run well on your own board or not?&lt;/P&gt;&lt;P&gt;Did the demo code work well on the FRDM-KE02 board or not?&lt;/P&gt;&lt;P&gt;FRDM-KEXX Driver Library package:&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp" title="https://www.nxp.com/webapp/sps/download/preDownload.jsp"&gt;https://www.nxp.com/webapp/sps/download/preDownload.jsp&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 06:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476355#M29004</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-27T06:02:48Z</dc:date>
    </item>
    <item>
      <title>Re: ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476356#M29005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The kexx_DRV projects as such do not run on my board unless I am debugging(very slow since I have 32khz crystal). They ran well on the freedom board. Similar is the project created by PE. Is my hardware the problem? But it's running smooth in debugging.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 09:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476356#M29005</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-27T09:23:44Z</dc:date>
    </item>
    <item>
      <title>Re: ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476357#M29006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy,&lt;/P&gt;&lt;P&gt;Now the PE project has started to running after flashing, but not after por. The kexx_DRV_lib projects still fail to start on por/after flashing. I think the reset circuitry is clean, I have .1uF cap at the reset pin. Voltage at the reset pin is stable.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 12:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476357#M29006</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-27T12:06:09Z</dc:date>
    </item>
    <item>
      <title>Re: ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476358#M29007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suraj,&lt;/P&gt;&lt;P&gt;I think the root cause is relate to the hardware circuit and you can go for a test again by following the steps below.&lt;/P&gt;&lt;P&gt;1. Just remain the mini-system after remove the stuffs on your own board;&lt;/P&gt;&lt;P&gt;2. Debug and program the KExx_DRV_lib projects to mini-system;&lt;/P&gt;&lt;P&gt;3. Check out the run result of the after programming and POR;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 01:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476358#M29007</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-28T01:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: ke02z run only in debug</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476359#M29008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeremy,&lt;/P&gt;&lt;P&gt;It worked. Thank you. I had capacitive load on some of the analog inputs(for filtering). Disconnected the inputs and its working fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 06:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ke02z-run-only-in-debug/m-p/476359#M29008</guid>
      <dc:creator>surajka</dc:creator>
      <dc:date>2016-04-28T06:18:51Z</dc:date>
    </item>
  </channel>
</rss>