<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How do I program a FRDM-K64F using a Cyclone Max and the PROGARM software?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474257#M28799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Scott Lyle:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The trace &lt;STRONG&gt;J11&lt;/STRONG&gt; MUST NOT be cut, only if you want to use the Freedom board as programmer for an external MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try again by placing the &lt;STRONG&gt; J11&lt;/STRONG&gt; jumper and let us know if the issue is not resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 21:30:10 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-12-09T21:30:10Z</dc:date>
    <item>
      <title>How do I program a FRDM-K64F using a Cyclone Max and the PROGARM software?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474256#M28798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a FRDM-K64F development board that I would like to program using the Cyclone Max via the PROGARM software. My goal is to come up with a way to program a MK24FN1M0VDC12 processor on a custom PCB we designed using the 0.5", 10 pin SWD header.&amp;nbsp; Before trying to debug whether or not our PCB design is correct, I would like to first make sure the process for programming a Kinetis CPU this way is correct using the FRDM board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So far I have downloaded all of the programming algorithms.&amp;nbsp; I plug the cable into port E on the Cyclone Max and use the Cyclone Max JTAG/SWD adapter board to interface to the 0.05", 10 pin SWD connector J9 on the FRDM board.&amp;nbsp; I have tried the jumper on the adapter board in both positions.&amp;nbsp; I have cut the trace under J11 as directed in the manual and schematics.&amp;nbsp; Each cable has the red wire going to pin 1 of the appropriate connector.&amp;nbsp; I am powering the FRDM board through J26.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the PROGARM software use the default settings and select either the freescale_k64fn1m0m12_1x32x256k_pflash.arp or freescale_k64fn1m0m12ws_1x32x256k_pflash.arp programming algorithm I get the message "Initializing.&amp;nbsp; Cannot enter background mode.&amp;nbsp; Check connections."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your time!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 21:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474256#M28798</guid>
      <dc:creator>scottlyle</dc:creator>
      <dc:date>2015-12-09T21:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: How do I program a FRDM-K64F using a Cyclone Max and the PROGARM software?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474257#M28799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Scott Lyle:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The trace &lt;STRONG&gt;J11&lt;/STRONG&gt; MUST NOT be cut, only if you want to use the Freedom board as programmer for an external MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try again by placing the &lt;STRONG&gt; J11&lt;/STRONG&gt; jumper and let us know if the issue is not resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 21:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474257#M28799</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-12-09T21:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: How do I program a FRDM-K64F using a Cyclone Max and the PROGARM software?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474258#M28800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the clarification on J11.&amp;nbsp; I have reconnected those two pins. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also found that I needed to upgrade my Cyclone Max software.&amp;nbsp; Unfortunately it is still not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now using the PROGACMP software.&amp;nbsp; I select either K64FN1M0M12 or K64FN1M0M12 as the device.&amp;nbsp; I found that if I power the board from either J26 or from the Cyclone Max that clicking "Connect (Reset)" just brings up the Connection Assistant again.&amp;nbsp; This is the same behavior if no device is present.&amp;nbsp; However, if I power the board through the other, non debug USB port it takes me into the CPOGACMP application and asks for an algorithm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point it acts the same way it did before.&amp;nbsp; No matter which of the two algorithms I select it gives me the same "Initializing.&amp;nbsp; Cannot enter background mode.&amp;nbsp; Check connections." error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 19:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474258#M28800</guid>
      <dc:creator>scottlyle</dc:creator>
      <dc:date>2015-12-10T19:07:00Z</dc:date>
    </item>
    <item>
      <title>Re: How do I program a FRDM-K64F using a Cyclone Max and the PROGARM software?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474259#M28801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I talked with PE Micro and found that there are traces under J8 and J12 that need to be cut to prevent the OpenSDA from interfering with the SWD port.&amp;nbsp; After cutting those traces I am now able to program the FRDM board with the Cyclone Max.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again for the help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 21:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-program-a-FRDM-K64F-using-a-Cyclone-Max-and-the-PROGARM/m-p/474259#M28801</guid>
      <dc:creator>scottlyle</dc:creator>
      <dc:date>2015-12-10T21:10:24Z</dc:date>
    </item>
  </channel>
</rss>