<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K82 freedom board doesn't power up. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473944#M28759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually the board is not powering on only. So it is not possible to get it into bootloader mode.&lt;BR /&gt;When I power it using the USB, the green power led doesn't light up..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Apr 2016 11:34:26 GMT</pubDate>
    <dc:creator>rushirajjawale</dc:creator>
    <dc:date>2016-04-28T11:34:26Z</dc:date>
    <item>
      <title>K82 freedom board doesn't power up.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473941#M28756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K82 freedom board doesn't power up. While I was installing the JLink open SDA bootloader to the board. It got disconnected from the laptop. And now it doesn't power up. The green power doesn't glow. I tried checking the power supply with a multimeter. It looks ok. Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Apr 2016 19:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473941#M28756</guid>
      <dc:creator>rushirajjawale</dc:creator>
      <dc:date>2016-04-24T19:07:31Z</dc:date>
    </item>
    <item>
      <title>Re: K82 freedom board doesn't power up.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473942#M28757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer below thread for the same issue:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389254"&gt;In need for a Jlink bootloader MK20DX128VFM5 project for the FRDM-K82F board&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 07:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473942#M28757</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-04-27T07:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: K82 freedom board doesn't power up.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473943#M28758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do a test with FRDM-K82F board and it need to upload &lt;A href="https://www.segger.com/opensda.html"&gt;J-Link OpenSDA V2.1 firmware&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Customer can let board enter into Bootloader mode again, then plug the firmware file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 09:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473943#M28758</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-04-27T09:56:18Z</dc:date>
    </item>
    <item>
      <title>Re: K82 freedom board doesn't power up.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473944#M28759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually the board is not powering on only. So it is not possible to get it into bootloader mode.&lt;BR /&gt;When I power it using the USB, the green power led doesn't light up..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 11:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473944#M28759</guid>
      <dc:creator>rushirajjawale</dc:creator>
      <dc:date>2016-04-28T11:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: K82 freedom board doesn't power up.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473945#M28760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the USB port you are using.&lt;/P&gt;&lt;P&gt;The OpenSDA is powered by P5V_SDA with J5 USB port;&lt;/P&gt;&lt;P&gt;When you power the board with J11 USB port, which doesn't provide power to OpenSDA, only power K82 chip.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 02:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-freedom-board-doesn-t-power-up/m-p/473945#M28760</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-04-29T02:05:11Z</dc:date>
    </item>
  </channel>
</rss>