<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL70 RTC not running</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL70-RTC-not-running/m-p/473914#M28755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Discovered the problem.&amp;nbsp; Internal Loading Capacitance needed to be set in the RTC_CR register.&amp;nbsp;&amp;nbsp; The CPU board does not have any cap's populated in the external clock circuit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Apr 2016 20:21:35 GMT</pubDate>
    <dc:creator>philmac</dc:creator>
    <dc:date>2016-04-25T20:21:35Z</dc:date>
    <item>
      <title>KL70 RTC not running</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL70-RTC-not-running/m-p/473913#M28754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Whenever I attempt to read the time from the RTC it will always return the same value that I originally set it to.&amp;nbsp; It does not update.&amp;nbsp;&amp;nbsp; I have checked the external clock and it is producing a 32khz signal into the EXTAL32 pins.&amp;nbsp;&amp;nbsp; I have checked the BSP code and it is executing the _rtc_init function on startup.&amp;nbsp; I have traced the code and it does get into that function.&amp;nbsp; As I said I can write and read the RTC and it retains the time that I sent to it.&amp;nbsp;&amp;nbsp; Any other ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 15:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL70-RTC-not-running/m-p/473913#M28754</guid>
      <dc:creator>philmac</dc:creator>
      <dc:date>2016-04-25T15:32:41Z</dc:date>
    </item>
    <item>
      <title>Re: KL70 RTC not running</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL70-RTC-not-running/m-p/473914#M28755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Discovered the problem.&amp;nbsp; Internal Loading Capacitance needed to be set in the RTC_CR register.&amp;nbsp;&amp;nbsp; The CPU board does not have any cap's populated in the external clock circuit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Apr 2016 20:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL70-RTC-not-running/m-p/473914#M28755</guid>
      <dc:creator>philmac</dc:creator>
      <dc:date>2016-04-25T20:21:35Z</dc:date>
    </item>
  </channel>
</rss>