<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックsd card</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/sd-card/m-p/472760#M28658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with kinetis k60 and I'm develomping an application that uses an sd card by spi. I check the sd card presence, but I'd like evalute if sd card is working&amp;nbsp; correctly or Not. I want to do this because sometimes when I turn on the device, the sd card is locked and it is impossibile to comunicate with it unti I cut its power supply. Does someone help&amp;nbsp; me?&lt;/P&gt;&lt;P&gt;Many&amp;nbsp; thanks in advance for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Stefano &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 21:12:02 GMT</pubDate>
    <dc:creator>chobin</dc:creator>
    <dc:date>2015-12-09T21:12:02Z</dc:date>
    <item>
      <title>sd card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/sd-card/m-p/472760#M28658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with kinetis k60 and I'm develomping an application that uses an sd card by spi. I check the sd card presence, but I'd like evalute if sd card is working&amp;nbsp; correctly or Not. I want to do this because sometimes when I turn on the device, the sd card is locked and it is impossibile to comunicate with it unti I cut its power supply. Does someone help&amp;nbsp; me?&lt;/P&gt;&lt;P&gt;Many&amp;nbsp; thanks in advance for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Stefano &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 21:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/sd-card/m-p/472760#M28658</guid>
      <dc:creator>chobin</dc:creator>
      <dc:date>2015-12-09T21:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: sd card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/sd-card/m-p/472761#M28659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K60 product provides ESDHC interface could using to connect with SDCARD, while customer also could using SPI to connect SDCARD.&lt;/P&gt;&lt;P&gt;We have SPI SDCARD example demo based on MQX RTOS, which could be downloaded from &lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/more-processors/coldfire-plus-coldfire-mcus-mpus/coldfire-plus-mcus/mqx-software-solutions:MQX"&gt;here&lt;/A&gt; (the latest version is V4.2).&lt;/P&gt;&lt;P&gt;Customer could find TWR-K21D50M board sdcard demo is using SPI mode, the related software could be found at below folder:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard\build\iar\mfs_sdcard_twrk21d50m&lt;/P&gt;&lt;P&gt;In the &amp;lt;twrk21d50m.h&amp;gt; file of BSP project, which using SPI1 as SDCARD interface:&lt;/P&gt;&lt;P&gt;/*-----------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;**&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SDCARD&lt;/P&gt;&lt;P&gt;*/&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_SPI_CHANNEL&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "spi1:"&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_GPIO_DETECT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_C | GPIO_PIN5)&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_GPIO_PROTECT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_A | GPIO_PIN17)&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_DETECT_MUX_GPIO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (LWGPIO_MUX_C5_GPIO)&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_PROTECT_MUX_GPIO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (LWGPIO_MUX_A17_GPIO)&lt;/P&gt;&lt;P&gt;#define BSP_SDCARD_SPI_CS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer can refer this demo software.&lt;/P&gt;&lt;P&gt;The TWR-K21D50M board related resource could be found at &lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/tower-development-boards/mcu-and-processor-modules/kinetis-modules/kinetis-k21-50-mhz-mcu-tower-system-module:TWR-K21D50M"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Dec 2015 07:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/sd-card/m-p/472761#M28659</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-12-10T07:47:33Z</dc:date>
    </item>
  </channel>
</rss>