<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Cannot connect to FRDM-KE04Z, frustrated!</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472089#M28559</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What comes from the NXP FRDM-KE04Z page for CMSIS-DAP is "CMSIS-DAP_OpenSDA.S19"&amp;nbsp; Not a .SDA file, which is mysterious but OK.&amp;nbsp; I tried plunking the file onto the board after putting the board into BOOTLOADER mode, but nothing happened - at least, nothing good.&amp;nbsp; Can you tell me how you would expect this to work (each step) if starting with a pristine FRDM-KE04Z board?&amp;nbsp; Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 07:21:20 GMT</pubDate>
    <dc:creator>mikesilva</dc:creator>
    <dc:date>2016-04-05T07:21:20Z</dc:date>
    <item>
      <title>Cannot connect to FRDM-KE04Z, frustrated!</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472086#M28556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just spent a terrible, awful, horrible week trying to connect my toolset to a FRDM-KE04Z.&amp;nbsp; Details:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) My development platform is an iMac, which also runs Windows 10 via Parallels.&lt;/P&gt;&lt;P&gt;2) Toolset is Rowley Crossworks, which I've used for years with other controller families.&amp;nbsp; For the KE04Z board it offers connections via Segger J-Link, P&amp;amp;EMicro, and CMSIS-DAP (among many others).&lt;/P&gt;&lt;P&gt;3) I can run Crossworks under OS-X or Windows.&amp;nbsp; I'd prefer OS-X, but I'll run under Windows if I have to.&lt;/P&gt;&lt;P&gt;4) I have no problem in either OS seeing the KE04Z board in Bootloader mode&lt;/P&gt;&lt;P&gt;5) I can drag-download any of the 3 OpenSDA apps found in the Quick Start package with apparent success.&lt;/P&gt;&lt;P&gt;6) I can also drag-download the Segger OpenSDA file with apparent success.&lt;/P&gt;&lt;P&gt;7) I believe I have installed any required drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But under no circumstances have I been able to connect to the target board using any of the 3 protocols.&amp;nbsp; Using either OS.&amp;nbsp; After an entire week of fussing around!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I sense that there is something vague in the instructions that I am not understanding.&amp;nbsp; I really need some help.&amp;nbsp; The alternative is abandoning the Kinetis family altogether.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Apr 2016 17:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472086#M28556</guid>
      <dc:creator>mikesilva</dc:creator>
      <dc:date>2016-04-02T17:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to FRDM-KE04Z, frustrated!</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472087#M28557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;P&gt;For Crossworks you need to use the DMSIS-DAP debugger.&lt;/P&gt;&lt;P&gt;If you have problems with it, it is best to contact Rowley since they may be able to help best.&lt;/P&gt;&lt;P&gt;You could also install IAR KickStart since this is adequate for the KE04 - it works fine with DEBUG-APP_Pemicro_v107.SDA. Also NXP's KDS will do it.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Apr 2016 23:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472087#M28557</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-04-02T23:54:37Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to FRDM-KE04Z, frustrated!</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472088#M28558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can have a look to:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/356542"&gt;openSDA for Mac OS X&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/357363"&gt;OpenOCD, Mac OS, FRDM-K64F&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 02:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472088#M28558</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-05T02:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to FRDM-KE04Z, frustrated!</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472089#M28559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What comes from the NXP FRDM-KE04Z page for CMSIS-DAP is "CMSIS-DAP_OpenSDA.S19"&amp;nbsp; Not a .SDA file, which is mysterious but OK.&amp;nbsp; I tried plunking the file onto the board after putting the board into BOOTLOADER mode, but nothing happened - at least, nothing good.&amp;nbsp; Can you tell me how you would expect this to work (each step) if starting with a pristine FRDM-KE04Z board?&amp;nbsp; Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 07:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472089#M28559</guid>
      <dc:creator>mikesilva</dc:creator>
      <dc:date>2016-04-05T07:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to FRDM-KE04Z, frustrated!</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472090#M28560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;The application note illustrates the way to implement the OpenSDA interface, so I'd highly recommend you to refer to it for details.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/09/20/opensda-on-the-freedom-kl25z-board/" title="http://mcuoneclipse.com/2012/09/20/opensda-on-the-freedom-kl25z-board/"&gt;OpenSDA on the Freedom KL25Z Board | MCU on Eclipse&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 09:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-FRDM-KE04Z-frustrated/m-p/472090#M28560</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-05T09:43:41Z</dc:date>
    </item>
  </channel>
</rss>