<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV5x processor and external memory.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472047#M28554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mario,&lt;/P&gt;&lt;P&gt;In my opinion, the KV5x is good choose.&lt;/P&gt;&lt;P&gt;I've attached the datasheet of the KV5x, and you can check the detail characteristics in the attachment.&lt;/P&gt;&lt;P&gt;However you should use the Flexbus module to interface a external RAM device, as the KV5x hasn't enough RAM size to meet your requirement.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Feb 2016 02:45:29 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-02-19T02:45:29Z</dc:date>
    <item>
      <title>KV5x processor and external memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472046#M28553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm interested in a TWR-KV58F22M board using a KV5x processor. For my application i need to sample in parallel 4 ADCs every at 2-3Msps. I need to store the data, so i need 64MByte memory fast enough storing roughly 16MBytes/s. Is it possible? Which memory modules are suitable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 21:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472046#M28553</guid>
      <dc:creator>mariod</dc:creator>
      <dc:date>2016-02-18T21:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: KV5x processor and external memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472047#M28554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mario,&lt;/P&gt;&lt;P&gt;In my opinion, the KV5x is good choose.&lt;/P&gt;&lt;P&gt;I've attached the datasheet of the KV5x, and you can check the detail characteristics in the attachment.&lt;/P&gt;&lt;P&gt;However you should use the Flexbus module to interface a external RAM device, as the KV5x hasn't enough RAM size to meet your requirement.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 02:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472047#M28554</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-02-19T02:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: KV5x processor and external memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472048#M28555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answere....i'm still confused about the Flexbus interface. Which kind of RAM modules can i connect? All other things are reall good...if memory type is clear, i will order one....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 16:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV5x-processor-and-external-memory/m-p/472048#M28555</guid>
      <dc:creator>mariod</dc:creator>
      <dc:date>2016-02-19T16:58:52Z</dc:date>
    </item>
  </channel>
</rss>