<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Project USB_CDC.eww</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471189#M28473</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!! Thank you very much!!&lt;/P&gt;&lt;P&gt;I installed the evaluation version (so, I don't have access to the example files) for understanding the glucometer application, and then migrating to a free software... But, actually I cannot even load the software from MED-GLU nor MEDICAL-GUI. Indeed, my board TWR-K53-N512 is not recognized.&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 19:40:51 GMT</pubDate>
    <dc:creator>sandraarias</dc:creator>
    <dc:date>2016-04-26T19:40:51Z</dc:date>
    <item>
      <title>Project USB_CDC.eww</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471187#M28471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m trying to load IAR project on K53 for MED-GLU, the application note does not include the USB_CDC.eww… Could you please help me!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Apr 2016 00:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471187#M28471</guid>
      <dc:creator>sandraarias</dc:creator>
      <dc:date>2016-04-23T00:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: Project USB_CDC.eww</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471188#M28472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Sandra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this is the scenario, previously, the IAR has examples, which located at the directory after you install IAR.&lt;/P&gt;&lt;P&gt;C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\examples&lt;/P&gt;&lt;P&gt;If the IAR install a lof examples, the IAR package will be too large, now, the example are removed as the text.txt says:&lt;/P&gt;&lt;P&gt;Pls read the "readme.txt" located at :C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\examples&lt;/P&gt;&lt;P&gt;Now, the KSDK has the cdc example if you have installed the KSSK1.3, pls refer to the CDC example:&lt;/P&gt;&lt;P&gt;D:\Freescale\KSDK_1.3.0\examples\frdmk64f\demo_apps\usb\device\cdc\virtual_com\mqx\iar&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"readme.txt" says:&lt;/P&gt;&lt;P&gt;To increase the download and installation speed for IAR Embedded Workbench,&lt;/P&gt;&lt;P&gt;the example projects are no longer part of the installed product.&lt;/P&gt;&lt;P&gt;Example projects can be downloaded on a per chip manufacturer basis using&lt;/P&gt;&lt;P&gt;the Examples page in the IAR Embedded Workbench Information Center.&lt;/P&gt;&lt;P&gt;In cases when no internet access is available, the examples can also be unpacked from the DVD installation media. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 07:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471188#M28472</guid>
      <dc:creator>xiangjunrong</dc:creator>
      <dc:date>2016-04-26T07:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: Project USB_CDC.eww</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471189#M28473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!! Thank you very much!!&lt;/P&gt;&lt;P&gt;I installed the evaluation version (so, I don't have access to the example files) for understanding the glucometer application, and then migrating to a free software... But, actually I cannot even load the software from MED-GLU nor MEDICAL-GUI. Indeed, my board TWR-K53-N512 is not recognized.&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 19:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Project-USB-CDC-eww/m-p/471189#M28473</guid>
      <dc:creator>sandraarias</dc:creator>
      <dc:date>2016-04-26T19:40:51Z</dc:date>
    </item>
  </channel>
</rss>