<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: System oscillator will not start</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469225#M28346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the External Crystal/Resonator Connections section, it illustrates the various external crystal/resonator connections of the corresponded oscillator mode.&lt;/P&gt;&lt;P&gt;And please refer to it in details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 08:51:00 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-12-09T08:51:00Z</dc:date>
    <item>
      <title>System oscillator will not start</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469222#M28343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the FRDM-K22F ( MK22FN512VLH12 ), and trying to use the external crystall.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After setting up the HGO = 1, Range = 1 and EREFS = 1, and selecting CLKS = 2 I would assume that the oscillator should start, but nothing happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified that R57 is not present on the PCB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 11:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469222#M28343</guid>
      <dc:creator>aune</dc:creator>
      <dc:date>2015-12-08T11:21:37Z</dc:date>
    </item>
    <item>
      <title>Re: System oscillator will not start</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469223#M28344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I don't set the HGO = 1, but leave this at 0, it works. ANyone got a good explanation why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 12:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469223#M28344</guid>
      <dc:creator>aune</dc:creator>
      <dc:date>2015-12-08T12:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: System oscillator will not start</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469224#M28345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gain setting must match with the HW.&lt;/P&gt;&lt;P&gt;If the crystal is not loaded (no loading capacitors or feedback resistor) the&lt;SPAN style="text-decoration: underline;"&gt; low gain&lt;/SPAN&gt; is correct. &lt;EM&gt;Setting high gain will be wrong and not work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;If the crystal is loaded (with loading capacitors and a feedback resistor) the &lt;SPAN style="text-decoration: underline;"&gt;high gain&lt;/SPAN&gt; is correct. &lt;EM&gt;Setting low gain will be wrong and not work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Some Freescale boards require high gain and some require low gain.&lt;/P&gt;&lt;P&gt;If it is not clear from the circuit see which one works and use that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 13:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469224#M28345</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-12-08T13:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: System oscillator will not start</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469225#M28346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the External Crystal/Resonator Connections section, it illustrates the various external crystal/resonator connections of the corresponded oscillator mode.&lt;/P&gt;&lt;P&gt;And please refer to it in details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 08:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469225#M28346</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-12-09T08:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: System oscillator will not start</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469226#M28347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the explanation, makes sense.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you said, I have no external feedback resistor, so when setting HGO = 0, the oscillator started up just fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 09:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-oscillator-will-not-start/m-p/469226#M28347</guid>
      <dc:creator>aune</dc:creator>
      <dc:date>2015-12-09T09:56:11Z</dc:date>
    </item>
  </channel>
</rss>