<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKW22D512 - How to use the internal 1.2V reference for ADC? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW22D512-How-to-use-the-internal-1-2V-reference-for-ADC/m-p/469085#M28339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GLAUCIO GUIA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VREF is a module that has to be enable, hence, it is not always enable, if you want to do this in KSDK you can do it with CLOCK_SYS_EnableVrefClock(0); before you initialize your ADC: NOTE: PMC_REGSC[BGEN] bit must be set if the VREF regulator is required to remain operating in VLPx modes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since VREF is not related with VREFH and VREFL pins, so yes, there is not problem if you use it as ADC reference. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this help!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jun 2016 21:57:49 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2016-06-03T21:57:49Z</dc:date>
    <item>
      <title>MKW22D512 - How to use the internal 1.2V reference for ADC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW22D512-How-to-use-the-internal-1-2V-reference-for-ADC/m-p/469084#M28338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Is the 1.2V internal reference always enabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the ADC16_DRV_Init() function (Kinetis SDK) for ADC module initialization. In the parameter refVoltSrc I'm using the value kAdc16RefVoltSrcOfValt. Is it enough to use the internal 1.2V as ADC reference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;adcUserConfig.refVoltSrc = kAdc16RefVoltSrcOfValt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Glaucio Guia.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 06:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW22D512-How-to-use-the-internal-1-2V-reference-for-ADC/m-p/469084#M28338</guid>
      <dc:creator>glaucioguia</dc:creator>
      <dc:date>2016-06-01T06:11:08Z</dc:date>
    </item>
    <item>
      <title>Re: MKW22D512 - How to use the internal 1.2V reference for ADC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW22D512-How-to-use-the-internal-1-2V-reference-for-ADC/m-p/469085#M28339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GLAUCIO GUIA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VREF is a module that has to be enable, hence, it is not always enable, if you want to do this in KSDK you can do it with CLOCK_SYS_EnableVrefClock(0); before you initialize your ADC: NOTE: PMC_REGSC[BGEN] bit must be set if the VREF regulator is required to remain operating in VLPx modes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since VREF is not related with VREFH and VREFL pins, so yes, there is not problem if you use it as ADC reference. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this help!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 21:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKW22D512-How-to-use-the-internal-1-2V-reference-for-ADC/m-p/469085#M28339</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-06-03T21:57:49Z</dc:date>
    </item>
  </channel>
</rss>