<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Float and Double on K65</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Float-and-Double-on-K65/m-p/468973#M28334</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Goran,&lt;/P&gt;&lt;P&gt;As you know that the K65 with FPU module can only do single precision float operation with hardware, and the DSP instructions in the Cortex-M4 only support integer or fixed point(fractional data) operation. Both the FPU and DSP instruction do not help to operate the double float operation.&lt;/P&gt;&lt;P&gt;Fortunately, the C compilers support double float operation by software simulation, but it takes a long time.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Mar 2016 04:32:34 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-03-11T04:32:34Z</dc:date>
    <item>
      <title>Float and Double on K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Float-and-Double-on-K65/m-p/468972#M28333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using K65 in life science project. My customer insist to use double. &lt;/P&gt;&lt;P&gt;The built in single precision FPU + DSP will help or not?&lt;/P&gt;&lt;P&gt;Also, what is the impact on the processing speed?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 19:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Float-and-Double-on-K65/m-p/468972#M28333</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-03-10T19:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: Float and Double on K65</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Float-and-Double-on-K65/m-p/468973#M28334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Goran,&lt;/P&gt;&lt;P&gt;As you know that the K65 with FPU module can only do single precision float operation with hardware, and the DSP instructions in the Cortex-M4 only support integer or fixed point(fractional data) operation. Both the FPU and DSP instruction do not help to operate the double float operation.&lt;/P&gt;&lt;P&gt;Fortunately, the C compilers support double float operation by software simulation, but it takes a long time.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 04:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Float-and-Double-on-K65/m-p/468973#M28334</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-03-11T04:32:34Z</dc:date>
    </item>
  </channel>
</rss>