<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kwikstik SDcard witg SPI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-SDcard-witg-SPI/m-p/468906#M28327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which revision of the KWIKSTIK do you have?&lt;/P&gt;&lt;P&gt;Rev. 4 has errors which don't allow the SD card to be used without reworking - which is generaly not practical (neither SPI nor SHDC)&lt;/P&gt;&lt;P&gt;Rev. 5 is OK for SDHC mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore it makes sense to use SDHC if you have a revision 5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a reference here that will allow you to test the SD card operation:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.utasker.com/kinetis/KWIKSTIK.html" rel="nofollow"&gt;http://www.utasker.com/kinetis/KWIKSTIK.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jan 2016 14:04:50 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2016-01-27T14:04:50Z</dc:date>
    <item>
      <title>Kwikstik SDcard witg SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-SDcard-witg-SPI/m-p/468905#M28326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I would like to communicate kwikstik &amp;lt;--&amp;gt; SDcard over SPI. But it not going, the SDcard is in sockot on kwikstik.&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14538870231707179 jive_text_macro" data-renderedposition="29_8_1232_720" jivemacro_uid="_14538870231707179"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;char spi_send(char spiMsg)&amp;nbsp; &lt;/P&gt;&lt;P&gt;{&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; char temp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(!(SPI1_SR &amp;amp; SPI_SR_TFFF_MASK));&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&amp;nbsp; //While buffer is not empty do nothing&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_PUSHR = spiMsg &amp;amp; 0xff;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Write char to SPI&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(!(SPI1_SR &amp;amp; SPI_SR_RFDF_MASK))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("nop");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp = SPI1_POPR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_SR = SPI_SR_TFFF_MASK | (SPI1_SR &amp;amp; SPI_SR_RFDF_MASK);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return temp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void init_SPI1()&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //SPI1 for SDcard&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Turn on clock to module&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC6 |= SIM_SCGC6_SPI1_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Enable SPI1 clock&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR6 = PORT_PCR_MUX(1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PDDR |= 1&amp;lt;&amp;lt;6;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PSOR |= 1&amp;lt;&amp;lt;6;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Enable 3.3V to SDcard, see kwikstik schematics&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR4 = PORT_PCR_MUX(0x2);&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set PTE4 to mux 2 [SPI1_PCS0]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR1 = PORT_PCR_MUX(0x2);&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set PTE3 to mux 2 [SPI1_MOSI?]&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR2 = PORT_PCR_MUX(0x2);&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set PTE1 to mux 2 [SPI1_SCK]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR3 = PORT_PCR_MUX(0x2);&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set PTE2 to mux 2 [SPI1_MISO?]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTE_PCR4 = PORT_PCR_MUX(1);&amp;nbsp;&amp;nbsp;&amp;nbsp; //PORTE1 is CS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PDDR |= 1&amp;lt;&amp;lt;4;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PORTE1 is output, for CS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_MCR = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_MCR |= (SPI_MCR_MSTR_MASK | SPI_MCR_HALT_MASK | SPI_MCR_DCONF(0x0) | SPI_MCR_CLR_TXF_MASK | SPI_MCR_CLR_RXF_MASK);&amp;nbsp;&amp;nbsp; //Set SPI1 to Master &amp;amp; SS pin to auto SS&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_TCR =&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_TCR_SPI_TCNT(0x0);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_CTAR0 = SPI_CTAR_FMSZ(7);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_CTAR0 |= (SPI_CTAR_PBR(3) | SPI_CTAR_BR(10));&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_CTAR1 = SPI_CTAR_FMSZ(7);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_CTAR1 |= (SPI_CTAR_PBR(3) | SPI_CTAR_BR(10));&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI1_MCR &amp;amp;= ~SPI_MCR_HALT_MASK;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I doing wrong? Thank You!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 09:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-SDcard-witg-SPI/m-p/468905#M28326</guid>
      <dc:creator>mqxman</dc:creator>
      <dc:date>2016-01-27T09:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: Kwikstik SDcard witg SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-SDcard-witg-SPI/m-p/468906#M28327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which revision of the KWIKSTIK do you have?&lt;/P&gt;&lt;P&gt;Rev. 4 has errors which don't allow the SD card to be used without reworking - which is generaly not practical (neither SPI nor SHDC)&lt;/P&gt;&lt;P&gt;Rev. 5 is OK for SDHC mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore it makes sense to use SDHC if you have a revision 5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a reference here that will allow you to test the SD card operation:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.utasker.com/kinetis/KWIKSTIK.html" rel="nofollow"&gt;http://www.utasker.com/kinetis/KWIKSTIK.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 14:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kwikstik-SDcard-witg-SPI/m-p/468906#M28327</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-27T14:04:50Z</dc:date>
    </item>
  </channel>
</rss>