<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Is the ARM PRIMASK LSB used by the KL17 hardware?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-ARM-PRIMASK-LSB-used-by-the-KL17-hardware/m-p/468578#M28288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering, is the ARM PRIMASK least significant bit (controllable by using CPSID i or CPSIE i or __disable_irq() or __enable_irq()) ever used by the KL17's hardware?&amp;nbsp; Specifically, does the KL17 hardware use the PRIMASK LSB to control the inhibiting of interrupts? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, how does the KL17 inhibit interrupts - for example, when the KL17 is in an interrupt it disables that interrupt so as not to cause an infinite number of interrupt calls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Apr 2016 23:12:22 GMT</pubDate>
    <dc:creator>rickstuart</dc:creator>
    <dc:date>2016-04-21T23:12:22Z</dc:date>
    <item>
      <title>Is the ARM PRIMASK LSB used by the KL17 hardware?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-ARM-PRIMASK-LSB-used-by-the-KL17-hardware/m-p/468578#M28288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering, is the ARM PRIMASK least significant bit (controllable by using CPSID i or CPSIE i or __disable_irq() or __enable_irq()) ever used by the KL17's hardware?&amp;nbsp; Specifically, does the KL17 hardware use the PRIMASK LSB to control the inhibiting of interrupts? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, how does the KL17 inhibit interrupts - for example, when the KL17 is in an interrupt it disables that interrupt so as not to cause an infinite number of interrupt calls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 23:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-ARM-PRIMASK-LSB-used-by-the-KL17-hardware/m-p/468578#M28288</guid>
      <dc:creator>rickstuart</dc:creator>
      <dc:date>2016-04-21T23:12:22Z</dc:date>
    </item>
  </channel>
</rss>