<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K70 Can module: 32 or 64 mailbox? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467275#M28202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;I&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;just saw&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this in the&lt;/SPAN&gt; chapter §3.9.4 CAN Configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jan 2016 06:48:57 GMT</pubDate>
    <dc:creator>arnogir</dc:creator>
    <dc:date>2016-01-06T06:48:57Z</dc:date>
    <item>
      <title>K70 Can module: 32 or 64 mailbox?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467273#M28200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the K70 150MHz with MQX 4.2 and KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet of the K70 (Rev.3 November 2014) indicate only the register CANx_IMASK1/ CANx_IFLAG1, not the IMASK2/IFLAG2...&lt;/P&gt;&lt;P&gt;But in KDS3.0 with EmbSys Register I can visualise&amp;nbsp; IFLAG2/IMASK2.&lt;/P&gt;&lt;P&gt;But on Can Clock Turn on in BSP init (sim-&amp;gt;SCGC6 |= SIM_SCGC6_FLEXCAN0_MASK;)&lt;/P&gt;&lt;P&gt;only IFLAG1/IMASK1 are set to 0, IMASK2/IFLAG 2 not change and MASK2 stay to 0x80008000???&lt;/P&gt;&lt;P&gt;Also, in Datasheet §53.3.12 (CANx_CTRL2) on RFFN description, there is a table indicate how many remaining available mailboxes which can up to 64...&lt;/P&gt;&lt;P&gt;:smileyconfused:&lt;/P&gt;&lt;P&gt;So if there is realy 64 Maibox, the Clock turn on allow automaticcaly to Reset MASK/IFLAG1 to 0 but not the IMASK2/IFLAG2, in which case, MQX 4.2 has a bug by not setting the default value register to 0..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So are they 32 or 64 mb in K70&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 10:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467273#M28200</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2016-01-05T10:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: K70 Can module: 32 or 64 mailbox?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467274#M28201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K70 has two identical FlexCAN&amp;nbsp; modules.&lt;/P&gt;&lt;P&gt;Each FlexCAN module contains 16 message buffers.Wish it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 06:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467274#M28201</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-01-06T06:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: K70 Can module: 32 or 64 mailbox?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467275#M28202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;&lt;SPAN class="hps"&gt;I&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;just saw&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this in the&lt;/SPAN&gt; chapter §3.9.4 CAN Configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 06:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Can-module-32-or-64-mailbox/m-p/467275#M28202</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2016-01-06T06:48:57Z</dc:date>
    </item>
  </channel>
</rss>